<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC4337 UART0 IS HANGING WHEN CONNECTING WITH FTDI TTL232R</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-UART0-IS-HANGING-WHEN-CONNECTING-WITH-FTDI-TTL232R/m-p/600063#M23266</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-content-finding="Community" data-userid="293961" data-username="aravindmuttineni" href="https://community.nxp.com/people/aravindmuttineni"&gt;aravind muttineni&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and the opportunity to serve you.&lt;/P&gt;&lt;P&gt;The UART hanging issue is very typical and it can be caused by hardware or software design.&lt;/P&gt;&lt;P&gt;So I was wondering if you can describe the flow which triggers the issue happen definitely, then it can help me to figure out the root cause of the issue.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 04 Feb 2017 03:26:21 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2017-02-04T03:26:21Z</dc:date>
    <item>
      <title>LPC4337 UART0 IS HANGING WHEN CONNECTING WITH FTDI TTL232R</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-UART0-IS-HANGING-WHEN-CONNECTING-WITH-FTDI-TTL232R/m-p/600062#M23265</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are using LPC4337 controller in one of our project. UART0 i am using for configuration over by connectiong FTDI TTL232R to PC. Sometimes it is working sometimes the controller is hanging. What is the problem?.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Feb 2017 11:03:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-UART0-IS-HANGING-WHEN-CONNECTING-WITH-FTDI-TTL232R/m-p/600062#M23265</guid>
      <dc:creator>aravindmuttinen</dc:creator>
      <dc:date>2017-02-03T11:03:53Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4337 UART0 IS HANGING WHEN CONNECTING WITH FTDI TTL232R</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-UART0-IS-HANGING-WHEN-CONNECTING-WITH-FTDI-TTL232R/m-p/600063#M23266</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-content-finding="Community" data-userid="293961" data-username="aravindmuttineni" href="https://community.nxp.com/people/aravindmuttineni"&gt;aravind muttineni&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and the opportunity to serve you.&lt;/P&gt;&lt;P&gt;The UART hanging issue is very typical and it can be caused by hardware or software design.&lt;/P&gt;&lt;P&gt;So I was wondering if you can describe the flow which triggers the issue happen definitely, then it can help me to figure out the root cause of the issue.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 04 Feb 2017 03:26:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-UART0-IS-HANGING-WHEN-CONNECTING-WITH-FTDI-TTL232R/m-p/600063#M23266</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2017-02-04T03:26:21Z</dc:date>
    </item>
  </channel>
</rss>