<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FreeRTOS interrupts and peripherals in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/FreeRTOS-interrupts-and-peripherals/m-p/598667#M23184</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Dimitris,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You need to use the LPCOpen I2C etc peripherals drivers. Yes, you can port the code inside a task.&lt;/P&gt;&lt;P&gt;For interrupts, please check the "Special note for Cortex-M users" in the following FAQ page: &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freertos.org/FAQHelp.html"&gt;http://www.freertos.org/FAQHelp.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt; Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 20 Oct 2016 22:21:03 GMT</pubDate>
    <dc:creator>soledad</dc:creator>
    <dc:date>2016-10-20T22:21:03Z</dc:date>
    <item>
      <title>FreeRTOS interrupts and peripherals</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/FreeRTOS-interrupts-and-peripherals/m-p/598666#M23183</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have some basic questions about FreeRTOS and how to handle interrupts from peripherals.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In LPCOpen examples there are some examples about i2c, ssp etc peripherals.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In order to create an application with FreeRTOS than can read and write to multiple periherals like i2c and ssp&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Do i need different driver implementations of i2c and ssp?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. Do i just port the code inside a task of FreeRTOS form and call xTaskCreate of this task? Or a different implementaion is needed?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3. When a peripheral (a sensor) raises an i2c interrupt and normally let's say I2C1_IRQHandler was triggered. With FreeRTOS how can i manage interrupts?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am reading the FreeRTOS site and many tutorials but i need a basic guideline from scratch so that i can clear things up in my mind.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanx a lot.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Oct 2016 09:51:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/FreeRTOS-interrupts-and-peripherals/m-p/598666#M23183</guid>
      <dc:creator>dimitrissideris</dc:creator>
      <dc:date>2016-10-03T09:51:21Z</dc:date>
    </item>
    <item>
      <title>Re: FreeRTOS interrupts and peripherals</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/FreeRTOS-interrupts-and-peripherals/m-p/598667#M23184</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Dimitris,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You need to use the LPCOpen I2C etc peripherals drivers. Yes, you can port the code inside a task.&lt;/P&gt;&lt;P&gt;For interrupts, please check the "Special note for Cortex-M users" in the following FAQ page: &amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freertos.org/FAQHelp.html"&gt;http://www.freertos.org/FAQHelp.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt; Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Oct 2016 22:21:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/FreeRTOS-interrupts-and-peripherals/m-p/598667#M23184</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2016-10-20T22:21:03Z</dc:date>
    </item>
  </channel>
</rss>