<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: LPC43xx RTC: avoid reiniting after each Deep Power Down wakeup</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-RTC-How-to-avoid-reiniting-after-each-Deep-Power-Down/m-p/598583#M23160</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Look into the attached source code which comes from an example which realized several power-down/wakeup scenarios.&lt;BR /&gt;It's programmed in a pretty simple way, please let me know if this helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 27 Dec 2016 22:48:53 GMT</pubDate>
    <dc:creator>soledad</dc:creator>
    <dc:date>2016-12-27T22:48:53Z</dc:date>
    <item>
      <title>LPC43xx RTC: How to avoid reiniting after each Deep Power Down wakeup</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-RTC-How-to-avoid-reiniting-after-each-Deep-Power-Down/m-p/598582#M23159</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I have to sleep the LPC4337 MCU in a long time, so I use RTC wake up from Deep Power Pown mode, but there is an issue with RTC initializing:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As LPC43xx RTC Datasheet:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;The RTC is configured as follows:&lt;BR /&gt;• See Table 874 for clocking and power control. The 1 kHz output of the 32 kHz oscillator must be enabled in the CREG0 register in the CREG block (see Table 97).&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But this is clock is disabled after reset (wake-up):&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_5.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/9562i959B0DC77F814DC7/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_5.png" alt="pastedImage_5.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;This mean I have to enable these bits each bootup (wakeup) and reinitialize whole RTC?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So my questions is: Does RTC need to reinitialize fully after wakeup? If not, how to do that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PS. I did try to omit the initializing sequence on wake up, but in that case RTC alarm doesn't work any more so it doesn't wake up after second sleep (RTC time increases normally). I may miss somethings.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Kha Vo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 11 Dec 2016 04:58:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-RTC-How-to-avoid-reiniting-after-each-Deep-Power-Down/m-p/598582#M23159</guid>
      <dc:creator>KhaVo</dc:creator>
      <dc:date>2016-12-11T04:58:05Z</dc:date>
    </item>
    <item>
      <title>Re: LPC43xx RTC: avoid reiniting after each Deep Power Down wakeup</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-RTC-How-to-avoid-reiniting-after-each-Deep-Power-Down/m-p/598583#M23160</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Look into the attached source code which comes from an example which realized several power-down/wakeup scenarios.&lt;BR /&gt;It's programmed in a pretty simple way, please let me know if this helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Dec 2016 22:48:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-RTC-How-to-avoid-reiniting-after-each-Deep-Power-Down/m-p/598583#M23160</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2016-12-27T22:48:53Z</dc:date>
    </item>
    <item>
      <title>Re: LPC43xx RTC: avoid reiniting after each Deep Power Down wakeup</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-RTC-How-to-avoid-reiniting-after-each-Deep-Power-Down/m-p/598584#M23161</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sol,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your answer but it doesn't solve my problem!&lt;/P&gt;&lt;P&gt;I did make the RTC run and wake up from deep power-down, but the RTC need to re-init every time before enter sleep.&lt;/P&gt;&lt;P&gt;I need to keep RTC running (without renit) on next wake-up/sleep.&lt;/P&gt;&lt;P&gt;Do you have any idea for this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Kha Vo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Dec 2016 21:27:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC43xx-RTC-How-to-avoid-reiniting-after-each-Deep-Power-Down/m-p/598584#M23161</guid>
      <dc:creator>KhaVo</dc:creator>
      <dc:date>2016-12-28T21:27:04Z</dc:date>
    </item>
  </channel>
</rss>