<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC824 Hardware Modbus CRC calculation</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-Hardware-Modbus-CRC-calculation/m-p/598400#M23153</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am interested in trying to use the LPC824 CRC hardware to calculate the CRC for the Modbus protocol.&lt;/P&gt;&lt;P&gt;I use a 512 byte CRC lookup table for the fastest software calculations but now am using a little slower version that uses only a 16 byte table, all to save on the limited flash. It would be much better to use the hardware somehow and Modbus is a very popular serial protocol used on micro controllers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;I have seen that it may be possible on other hardware CRC blocks such as below&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void ModbusSlave::_crc_append(uint8_t* buffer, uint8_t* length)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; CRC0-&amp;gt;GPOLY_ACCESS16BIT.GPOLYL = 0x8005;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; CRC0-&amp;gt;CTRL = CRC_CTRL_WAS_MASK | CRC_CTRL_TOT(1) | CRC_CTRL_TOTR(1);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; CRC0-&amp;gt;ACCESS16BIT.DATAL = 0xFFFF;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; CRC0-&amp;gt;CTRL &amp;amp;= ~CRC_CTRL_WAS_MASK;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; for (int i=0; i&amp;lt;(*length); i++) {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CRC0-&amp;gt;ACCESS8BIT.DATALL = buffer[i];&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; buffer[*length] = CRC0-&amp;gt;ACCESS8BIT.DATALU;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; buffer[*length+1] = CRC0-&amp;gt;ACCESS8BIT.DATALL;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; *length = *length + 2;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My feeble attempt to duplicate this does not work&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;uint16_t CalcModbusChecksum(uint8_t* buffer, uint8_t* length)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp; uint16_t ret;&lt;BR /&gt;&amp;nbsp; uint8_t&amp;nbsp; len = *length;&lt;BR /&gt;&amp;nbsp; Chip_Clock_EnablePeriphClock(SYSCTL_CLOCK_CRC);&lt;BR /&gt;&amp;nbsp; Chip_CRC_SetPoly(CRC_MODE_POLY_CRC32,CRC_MODE_WRDATA_BIT_RVS|CRC_MODE_SUM_BIT_RVS);&lt;BR /&gt;&amp;nbsp; Chip_CRC_SetSeed(0x8005);&lt;BR /&gt;&amp;nbsp; Chip_CRC_Write16(0xFFFF);&lt;BR /&gt;&amp;nbsp; while (len--){&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; *((uint8_t *)&amp;amp;LPC_CRC-&amp;gt;WRDATA32) = *buffer++;&lt;BR /&gt;&amp;nbsp; }&lt;BR /&gt;&amp;nbsp; ret = (uint16_t)Chip_CRC_Sum();&lt;BR /&gt;&amp;nbsp; return ret;&lt;BR /&gt;} // CalcModbusChecksum&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help would be appreciated.&lt;/P&gt;&lt;P&gt;This would be very useful to add in the LPC Open code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 16 Nov 2016 08:51:59 GMT</pubDate>
    <dc:creator>kiryat8</dc:creator>
    <dc:date>2016-11-16T08:51:59Z</dc:date>
    <item>
      <title>LPC824 Hardware Modbus CRC calculation</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-Hardware-Modbus-CRC-calculation/m-p/598400#M23153</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am interested in trying to use the LPC824 CRC hardware to calculate the CRC for the Modbus protocol.&lt;/P&gt;&lt;P&gt;I use a 512 byte CRC lookup table for the fastest software calculations but now am using a little slower version that uses only a 16 byte table, all to save on the limited flash. It would be much better to use the hardware somehow and Modbus is a very popular serial protocol used on micro controllers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;I have seen that it may be possible on other hardware CRC blocks such as below&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void ModbusSlave::_crc_append(uint8_t* buffer, uint8_t* length)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; CRC0-&amp;gt;GPOLY_ACCESS16BIT.GPOLYL = 0x8005;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; CRC0-&amp;gt;CTRL = CRC_CTRL_WAS_MASK | CRC_CTRL_TOT(1) | CRC_CTRL_TOTR(1);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; CRC0-&amp;gt;ACCESS16BIT.DATAL = 0xFFFF;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; CRC0-&amp;gt;CTRL &amp;amp;= ~CRC_CTRL_WAS_MASK;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; for (int i=0; i&amp;lt;(*length); i++) {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; CRC0-&amp;gt;ACCESS8BIT.DATALL = buffer[i];&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; buffer[*length] = CRC0-&amp;gt;ACCESS8BIT.DATALU;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; buffer[*length+1] = CRC0-&amp;gt;ACCESS8BIT.DATALL;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; *length = *length + 2;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My feeble attempt to duplicate this does not work&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;uint16_t CalcModbusChecksum(uint8_t* buffer, uint8_t* length)&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp; uint16_t ret;&lt;BR /&gt;&amp;nbsp; uint8_t&amp;nbsp; len = *length;&lt;BR /&gt;&amp;nbsp; Chip_Clock_EnablePeriphClock(SYSCTL_CLOCK_CRC);&lt;BR /&gt;&amp;nbsp; Chip_CRC_SetPoly(CRC_MODE_POLY_CRC32,CRC_MODE_WRDATA_BIT_RVS|CRC_MODE_SUM_BIT_RVS);&lt;BR /&gt;&amp;nbsp; Chip_CRC_SetSeed(0x8005);&lt;BR /&gt;&amp;nbsp; Chip_CRC_Write16(0xFFFF);&lt;BR /&gt;&amp;nbsp; while (len--){&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; *((uint8_t *)&amp;amp;LPC_CRC-&amp;gt;WRDATA32) = *buffer++;&lt;BR /&gt;&amp;nbsp; }&lt;BR /&gt;&amp;nbsp; ret = (uint16_t)Chip_CRC_Sum();&lt;BR /&gt;&amp;nbsp; return ret;&lt;BR /&gt;} // CalcModbusChecksum&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help would be appreciated.&lt;/P&gt;&lt;P&gt;This would be very useful to add in the LPC Open code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Nov 2016 08:51:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC824-Hardware-Modbus-CRC-calculation/m-p/598400#M23153</guid>
      <dc:creator>kiryat8</dc:creator>
      <dc:date>2016-11-16T08:51:59Z</dc:date>
    </item>
  </channel>
</rss>