<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックDMX RDM Slave (AN11153) modification</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/DMX-RDM-Slave-AN11153-modification/m-p/598316#M23147</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The AN11153 describes a hardware for DMX &amp;nbsp;RDM (master/slave).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to remove the optocouplers and connect the directly to the power stage and DMX lines. Is it possible to make such modification without adding extra hardware like level inverters ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thiago&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 07 Jan 2017 17:29:10 GMT</pubDate>
    <dc:creator>thiagorodrigues</dc:creator>
    <dc:date>2017-01-07T17:29:10Z</dc:date>
    <item>
      <title>DMX RDM Slave (AN11153) modification</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/DMX-RDM-Slave-AN11153-modification/m-p/598316#M23147</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The AN11153 describes a hardware for DMX &amp;nbsp;RDM (master/slave).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to remove the optocouplers and connect the directly to the power stage and DMX lines. Is it possible to make such modification without adding extra hardware like level inverters ?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thiago&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 07 Jan 2017 17:29:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/DMX-RDM-Slave-AN11153-modification/m-p/598316#M23147</guid>
      <dc:creator>thiagorodrigues</dc:creator>
      <dc:date>2017-01-07T17:29:10Z</dc:date>
    </item>
    <item>
      <title>Re: DMX RDM Slave (AN11153) modification</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/DMX-RDM-Slave-AN11153-modification/m-p/598317#M23148</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Thiago,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Because of the distance between nodes, DMX512 transmitters and receivers require different power supplies. This will increase the impedance of the earth ground, making it more likely that ground currents from other sources will find their way into the link’s ground wire. Isolating the link reduces or even eliminates these problems so there is no recommended to remove the optocouplers.&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jan 2017 01:23:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/DMX-RDM-Slave-AN11153-modification/m-p/598317#M23148</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2017-01-10T01:23:56Z</dc:date>
    </item>
    <item>
      <title>Re: DMX RDM Slave (AN11153) modification</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/DMX-RDM-Slave-AN11153-modification/m-p/598318#M23149</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello soledad,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for you reply. I agree it is safer, I was thinking about saving a few bucks but...&lt;/P&gt;&lt;P&gt;In the SDK, only the .bin file is provided. I am relatively new to LPC world (used to AVR), I´m using the FlashMagic to flash the LPC but it only accepts .hex files. How can I convert it, or recompile it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 05 Mar 2017 23:10:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/DMX-RDM-Slave-AN11153-modification/m-p/598318#M23149</guid>
      <dc:creator>thiagorodrigues</dc:creator>
      <dc:date>2017-03-05T23:10:18Z</dc:date>
    </item>
  </channel>
</rss>