<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 LPC1788 lcd display  affect  capture interrupt</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-lcd-display-affect-capture-interrupt/m-p/517671#M2302</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by fire on Thu Sep 06 18:27:25 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;That the use of emwin516, display content by capturing the decoded, only capture a decoding display information, through the capture interrupt display information obtained is correct, as long as the information through the emwin516 interface function display out, capture interrupt is affected, one along the two times to capture interrupt, and capture register(CCR) value is the same as the capture the&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:28:52 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:28:52Z</dc:date>
    <item>
      <title>LPC1788 lcd display  affect  capture interrupt</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-lcd-display-affect-capture-interrupt/m-p/517671#M2302</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by fire on Thu Sep 06 18:27:25 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;That the use of emwin516, display content by capturing the decoded, only capture a decoding display information, through the capture interrupt display information obtained is correct, as long as the information through the emwin516 interface function display out, capture interrupt is affected, one along the two times to capture interrupt, and capture register(CCR) value is the same as the capture the&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:28:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-lcd-display-affect-capture-interrupt/m-p/517671#M2302</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:28:52Z</dc:date>
    </item>
  </channel>
</rss>