<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PWM and output No. 3 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/PWM-and-output-No-3/m-p/595842#M22892</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by xianghuiwang on Thu May 29 16:40:48 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi, Teslabox,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It is recommended to use the match registers that are not pinned out to control the PWM cycle length.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;MAT3 is not pin out and can not work as PWM output but can be used to set the PWM cycles.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;regards,&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:23:23 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:23:23Z</dc:date>
    <item>
      <title>PWM and output No. 3</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/PWM-and-output-No-3/m-p/595841#M22891</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by teslabox on Fri May 23 12:25:57 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi everyone,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I design a PCB with PWM on LPC1114 and I need to use PWM1.0 (PIO1.1/MAT0 Timer 1 32b), PWM1.1 (PIO1.2/MAT1 Timer 1 32b) and PWM1.3 (PIO1.4/MAT3 Timer 1 32b) outputs.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am reading an user manual of LPC1114 and I am wondering is it possible to use PWM1.3/MAT3 as PWM output?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In the user manual is written:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Chapter: 21.7.12&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Table: 342&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Rev.: 12.1&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;PWMEN3 PWM channel 3 enable&lt;BR /&gt;Note: It is recommended to use match channel 3 to set&lt;BR /&gt;the PWM cycle. &lt;/SPAN&gt;&lt;HR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:23:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/PWM-and-output-No-3/m-p/595841#M22891</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:23:22Z</dc:date>
    </item>
    <item>
      <title>Re: PWM and output No. 3</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/PWM-and-output-No-3/m-p/595842#M22892</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by xianghuiwang on Thu May 29 16:40:48 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi, Teslabox,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It is recommended to use the match registers that are not pinned out to control the PWM cycle length.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;MAT3 is not pin out and can not work as PWM output but can be used to set the PWM cycles.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;regards,&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:23:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/PWM-and-output-No-3/m-p/595842#M22892</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:23:23Z</dc:date>
    </item>
  </channel>
</rss>