<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックIs M0 core Bit banding capable?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Is-M0-core-Bit-banding-capable/m-p/595410#M22815</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by rui.araujo on Fri Jun 13 04:12:24 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I want to implement semaphores between the two cores using the bit banding region and the AHB&amp;nbsp; SRAM sections.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;My implementation works fine on the M4 core but it hards fault while accessing the alias region on the M0.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;is the M0 capable of bit banding on the LPC43xx?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If not, how should I implement semaphores between the two cores?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:21:50 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:21:50Z</dc:date>
    <item>
      <title>Is M0 core Bit banding capable?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Is-M0-core-Bit-banding-capable/m-p/595410#M22815</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by rui.araujo on Fri Jun 13 04:12:24 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I want to implement semaphores between the two cores using the bit banding region and the AHB&amp;nbsp; SRAM sections.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;My implementation works fine on the M4 core but it hards fault while accessing the alias region on the M0.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;is the M0 capable of bit banding on the LPC43xx?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If not, how should I implement semaphores between the two cores?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:21:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Is-M0-core-Bit-banding-capable/m-p/595410#M22815</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:21:50Z</dc:date>
    </item>
    <item>
      <title>Re: Is M0 core Bit banding capable?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Is-M0-core-Bit-banding-capable/m-p/595411#M22816</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by TheFallGuy on Fri Jun 13 04:40:39 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;There is a whole section in the UM10503 on inter process communication. See Chapter 2.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:21:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Is-M0-core-Bit-banding-capable/m-p/595411#M22816</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:21:50Z</dc:date>
    </item>
    <item>
      <title>Re: Is M0 core Bit banding capable?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Is-M0-core-Bit-banding-capable/m-p/595412#M22817</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by rocketdawg on Fri Jun 13 09:25:08 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;and M0 &amp;amp; M0+ cores do not have bit banding&amp;nbsp; (although ARM says it can be added in some cases)&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:21:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Is-M0-core-Bit-banding-capable/m-p/595412#M22817</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:21:51Z</dc:date>
    </item>
  </channel>
</rss>