<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic EEPROM with LPC4357: 180 MHz or 204 MHz in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/EEPROM-with-LPC4357-180-MHz-or-204-MHz/m-p/594930#M22726</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by capiman on Wed Jan 07 03:23:23 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Does someone know details about the maximum clock of EEPROM?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;According to LPC4357 user manual UM10503.pdf (version 1.8 from 28. January 2014, table 1153)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;"EEPROM BASE_M4_CLK CLK_M4_EEPROM up to 204 MHz"&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;According to errata sheet ES_LPC435X_3X_2X_1X_FLASH.pdf (Rev. 5 — 15 August 2014):&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Chapter 3.2 EEPROM.2&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;A 16 kB EEPROM is available on these parts which operates up to 180 MHz.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;"&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What is correct? Must CLK_M4_EEPROM be limited to 180 MHz or can it be driven with 204 MHz?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Or is it due to changes in register RWSTATE and WSTATE, so it can be used with 204 MHz instead of 180 MHz?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:22:17 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:22:17Z</dc:date>
    <item>
      <title>EEPROM with LPC4357: 180 MHz or 204 MHz</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/EEPROM-with-LPC4357-180-MHz-or-204-MHz/m-p/594930#M22726</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by capiman on Wed Jan 07 03:23:23 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Does someone know details about the maximum clock of EEPROM?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;According to LPC4357 user manual UM10503.pdf (version 1.8 from 28. January 2014, table 1153)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;"EEPROM BASE_M4_CLK CLK_M4_EEPROM up to 204 MHz"&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;According to errata sheet ES_LPC435X_3X_2X_1X_FLASH.pdf (Rev. 5 — 15 August 2014):&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Chapter 3.2 EEPROM.2&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;A 16 kB EEPROM is available on these parts which operates up to 180 MHz.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;"&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What is correct? Must CLK_M4_EEPROM be limited to 180 MHz or can it be driven with 204 MHz?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Or is it due to changes in register RWSTATE and WSTATE, so it can be used with 204 MHz instead of 180 MHz?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:22:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/EEPROM-with-LPC4357-180-MHz-or-204-MHz/m-p/594930#M22726</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:22:17Z</dc:date>
    </item>
    <item>
      <title>Re: EEPROM with LPC4357: 180 MHz or 204 MHz</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/EEPROM-with-LPC4357-180-MHz-or-204-MHz/m-p/594931#M22727</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by embd02161991 on Thu Jan 08 19:58:50 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The maximum clock of EEPROM is&amp;nbsp; 204 Mhz as mentioned in the UM.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for pointing out the mistake in Errata sheet. It will updated in the next revision.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;NXP Technical Support&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:22:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/EEPROM-with-LPC4357-180-MHz-or-204-MHz/m-p/594931#M22727</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:22:19Z</dc:date>
    </item>
  </channel>
</rss>