<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Need to configure pin P8_1 as GPIO interrupt in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Need-to-configure-pin-P8-1-as-GPIO-interrupt/m-p/594797#M22702</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by alston_gama on Fri May 30 01:34:08 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi ,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I want to configure pin &lt;/SPAN&gt;&lt;STRONG&gt;[u]P8.1 FUNC0 =&amp;gt; GPIO4[1][/u]&lt;/STRONG&gt;&lt;SPAN&gt; as GPIO interrupt.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have added lpc43xx_gpio.h and lpc43xx_gpio.c files to my project.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;and thinking of use below driver routine &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;/*********************************************************************//**&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; * @briefEnable GPIO interrupt (just used for P0.0-P0.30, P2.0-P2.13)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; * @param[in]portNumPort number to read value, should be: 0 or 2&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; * @param[in]bitValueValue that contains all bits on GPIO to enable,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; * should be in range from 0 to 0xFFFFFFFF.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; * @param[in]edgeStatestate of edge, should be:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; * - 0: Rising edge&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; * - 1: Falling edge&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; * @returnNone&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; **********************************************************************/&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;void GPIO_IntCmd(uint8_t portNum, uint32_t bitValue, uint8_t edgeState)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;but according to the description given &lt;/SPAN&gt;&lt;STRONG&gt;Port number to read value, should be: 0 or 2&lt;/STRONG&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So, does it mean pin P8.1 FUNC0 =&amp;gt; GPIO4[1] can not be used as GPIO interrupt pin?!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Note: I am using Embedded Artist LPC4357 dev kit and Embedded Artist LCD disply board ( EA LCD 004 ).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;P8_1 is used for touch interrupt.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&amp;nbsp; &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:21:21 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:21:21Z</dc:date>
    <item>
      <title>Need to configure pin P8_1 as GPIO interrupt</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Need-to-configure-pin-P8-1-as-GPIO-interrupt/m-p/594797#M22702</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by alston_gama on Fri May 30 01:34:08 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi ,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I want to configure pin &lt;/SPAN&gt;&lt;STRONG&gt;[u]P8.1 FUNC0 =&amp;gt; GPIO4[1][/u]&lt;/STRONG&gt;&lt;SPAN&gt; as GPIO interrupt.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have added lpc43xx_gpio.h and lpc43xx_gpio.c files to my project.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;and thinking of use below driver routine &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;/*********************************************************************//**&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; * @briefEnable GPIO interrupt (just used for P0.0-P0.30, P2.0-P2.13)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; * @param[in]portNumPort number to read value, should be: 0 or 2&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; * @param[in]bitValueValue that contains all bits on GPIO to enable,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; * should be in range from 0 to 0xFFFFFFFF.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; * @param[in]edgeStatestate of edge, should be:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; * - 0: Rising edge&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; * - 1: Falling edge&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; * @returnNone&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; **********************************************************************/&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;void GPIO_IntCmd(uint8_t portNum, uint32_t bitValue, uint8_t edgeState)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;...&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;but according to the description given &lt;/SPAN&gt;&lt;STRONG&gt;Port number to read value, should be: 0 or 2&lt;/STRONG&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So, does it mean pin P8.1 FUNC0 =&amp;gt; GPIO4[1] can not be used as GPIO interrupt pin?!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Note: I am using Embedded Artist LPC4357 dev kit and Embedded Artist LCD disply board ( EA LCD 004 ).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;P8_1 is used for touch interrupt.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&amp;nbsp; &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:21:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Need-to-configure-pin-P8-1-as-GPIO-interrupt/m-p/594797#M22702</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:21:21Z</dc:date>
    </item>
    <item>
      <title>Re: Need to configure pin P8_1 as GPIO interrupt</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Need-to-configure-pin-P8-1-as-GPIO-interrupt/m-p/594798#M22703</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by embd02161991 on Fri May 30 11:48:17 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any GPIO pin can be used as a pin interrupt. Hence, Pin P8_1 can be used as a GPIO interrupt pin. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;You can refer to GPIO Pin interrupt function in LPC18xx&amp;nbsp; and implement a similar one for your application. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Have you checked out the LPCOpen software platform examples? They have&amp;nbsp; the latest libraries.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Please visit :&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.lpcware.com%2Fcontent%2Fnxpfile%2Flpcopen-software-development-platform-lpc43xx-packages" rel="nofollow" target="_blank"&gt;http://www.lpcware.com/content/nxpfile/lpcopen-software-development-platform-lpc43xx-packages&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;NXP Technical support&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:21:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Need-to-configure-pin-P8-1-as-GPIO-interrupt/m-p/594798#M22703</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:21:22Z</dc:date>
    </item>
  </channel>
</rss>