<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC11U68 ADCs 2Ms/s</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11U68-ADCs-2Ms-s/m-p/593572#M22522</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;LPC11U68 ADCs claim to run at 2Ms/s, but I am seeing conversion times of &amp;gt;60 clock cycles at 48MHz (&amp;lt;1Ms/s). I'm running a SeqA with a single channel in Burst mode, with an IRQ handler in RAM reading results into a simple buffer. Can anyone point me at a code sample which can achieve the 2Ms/s. I've checked the clock divider is 0 and Vdda is 3.3V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers, Bob.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EDIT :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; I solved this issue using DMA. 2MHz was then achievable.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Jul 2016 15:47:19 GMT</pubDate>
    <dc:creator>bobbann</dc:creator>
    <dc:date>2016-07-20T15:47:19Z</dc:date>
    <item>
      <title>LPC11U68 ADCs 2Ms/s</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11U68-ADCs-2Ms-s/m-p/593572#M22522</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;LPC11U68 ADCs claim to run at 2Ms/s, but I am seeing conversion times of &amp;gt;60 clock cycles at 48MHz (&amp;lt;1Ms/s). I'm running a SeqA with a single channel in Burst mode, with an IRQ handler in RAM reading results into a simple buffer. Can anyone point me at a code sample which can achieve the 2Ms/s. I've checked the clock divider is 0 and Vdda is 3.3V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers, Bob.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EDIT :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; I solved this issue using DMA. 2MHz was then achievable.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jul 2016 15:47:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11U68-ADCs-2Ms-s/m-p/593572#M22522</guid>
      <dc:creator>bobbann</dc:creator>
      <dc:date>2016-07-20T15:47:19Z</dc:date>
    </item>
    <item>
      <title>Re: LPC11U68 ADCs 2Ms/s</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11U68-ADCs-2Ms-s/m-p/593573#M22523</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bob,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Thank you for your problem solutions sharing!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jingjing&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Aug 2016 03:03:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC11U68-ADCs-2Ms-s/m-p/593573#M22523</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2016-08-23T03:03:11Z</dc:date>
    </item>
  </channel>
</rss>