<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 LPC4300 PWM: UM &amp;lt;-&amp;gt; Silicon Inconsistency</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4300-PWM-UM-lt-gt-Silicon-Inconsistency/m-p/593349#M22488</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by GTA on Mon May 12 07:13:28 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using MCPWM functionality on the LPC4357, and when three phase AC mode is enabled (ACMODE=1, CON reg. bit 30) the UM v1.8 states:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;* "3-phase AC-mode on: All PWM channels use the timer-counter and period register of channel 0" (Table 798)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;* "In this mode the period value is identical for all three channels and is determined by LIM0" (32.8.7)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;* "The LIM1-2 registers are not used" (32.8.7)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This is however not correct, as e.g. LIM1 is used to determine the period of MCOA1 and B1 also when ACMODE=1.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;BR,&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:20:32 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:20:32Z</dc:date>
    <item>
      <title>LPC4300 PWM: UM &lt;-&gt; Silicon Inconsistency</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4300-PWM-UM-lt-gt-Silicon-Inconsistency/m-p/593349#M22488</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by GTA on Mon May 12 07:13:28 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using MCPWM functionality on the LPC4357, and when three phase AC mode is enabled (ACMODE=1, CON reg. bit 30) the UM v1.8 states:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;* "3-phase AC-mode on: All PWM channels use the timer-counter and period register of channel 0" (Table 798)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;* "In this mode the period value is identical for all three channels and is determined by LIM0" (32.8.7)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;* "The LIM1-2 registers are not used" (32.8.7)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This is however not correct, as e.g. LIM1 is used to determine the period of MCOA1 and B1 also when ACMODE=1.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;BR,&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:20:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4300-PWM-UM-lt-gt-Silicon-Inconsistency/m-p/593349#M22488</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:20:32Z</dc:date>
    </item>
  </channel>
</rss>