<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: SDRAM reads corrupted while LCD active.</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/SDRAM-reads-corrupted-while-LCD-active/m-p/592912#M22433</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by suckfish on Sat Dec 22 20:02:20 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Despite not having a clue I managed to solve it myself...&amp;nbsp; I was initialising the sdram controller after then lcd controller.&amp;nbsp; Which meant that the sdram controller was not idle whilst being configured... fixing that has everything working beautifully.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:18:43 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:18:43Z</dc:date>
    <item>
      <title>SDRAM reads corrupted while LCD active.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SDRAM-reads-corrupted-while-LCD-active/m-p/592911#M22432</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by suckfish on Sat Dec 22 16:07:55 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I've got a problem with SDRAM reads from the CPU getting corrupted while driving a LCD from SDRAM.&amp;nbsp; Any ideas?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;My first guess is a timing problem with the memory accesses, but I really don't have much of a clue how to debug this.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This is a custom board with LPC4357 and a 256Mb 16-bit SDRAM.&amp;nbsp; The display is 1024 by 640 TFT, 52.25MHz pixel clock.&amp;nbsp; I get the problem both in 16bpp and 8bpp modes.&amp;nbsp; The CPU and SDRAM are running at 96MHz.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The display output appears rock solid; no glitches.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The M4 CPU is running test code that reads and writes test patterns; it shows no problems without the LCD running, but with the LCD running it starts showing errors.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;My first guess was that I was running out of SDRAM bandwidth, but reducing from 16bpp to 8bpp appears to make no difference.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The memory test code is just:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; volatile unsigned * const sdram = (v32 *) 0x60000000;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; for (int i = 0; i != size; ++i)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; sdram&lt;/SPAN&gt;&lt;I&gt; = i * 0x02030401;&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; putchar ('\n');&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; for (int i = 0; i != size; ++i) {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; unsigned e = i * 0x02030401;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; unsigned v = sdram&lt;I&gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if (v != e)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf ("Memtest: Bugger @ %06x expect %08x got %08x\n",&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; i, e, v);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;BR /&gt;&lt;BR /&gt;Cheers,&lt;BR /&gt;Ralph.&lt;/I&gt;&lt;/I&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:18:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SDRAM-reads-corrupted-while-LCD-active/m-p/592911#M22432</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:18:42Z</dc:date>
    </item>
    <item>
      <title>Re: SDRAM reads corrupted while LCD active.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SDRAM-reads-corrupted-while-LCD-active/m-p/592912#M22433</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by suckfish on Sat Dec 22 20:02:20 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Despite not having a clue I managed to solve it myself...&amp;nbsp; I was initialising the sdram controller after then lcd controller.&amp;nbsp; Which meant that the sdram controller was not idle whilst being configured... fixing that has everything working beautifully.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:18:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SDRAM-reads-corrupted-while-LCD-active/m-p/592912#M22433</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:18:43Z</dc:date>
    </item>
  </channel>
</rss>