<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 LPC1788 144 pin QFP type: W-type IO having problem in input mode.</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-144-pin-QFP-type-W-type-IO-having-problem-in-input-mode/m-p/517524#M2222</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by awadhesh on Thu Sep 04 04:06:41 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I want to interface micro SD card to ssp1 on pin 113, 112, 111, 109. But I had checked that problem in MISO pin i.e. 111(P0.8) not receiving anything from SD card. I checked it and there are data on that pin on oscilloscope.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Now I am going to check that&amp;nbsp; this pin can work in input mode or not. But it is always low whatever voltage applied on pin. After that I check the details of this pin, I got that these are W-type pin P0.7, P0.8, P0.9. I do same on all these pin, but these never read applied logic voltage.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;After I configured these as output and making these to high and low with some delays to blink four leds. All leds are blinking as per expectation. But when I read PIN register, only changing is in P0.6, which is D-type, all W-type cannot read these are always low, even connected leds are blinking. I configured these pins in every setting like-pull up, pull down, filter enable/disable, hys enable/disable etc, but never get result. code is here.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;========================================================================&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_IOCON-&amp;gt;P0_6 = 0x00;//SSEL-&amp;gt;SPI&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_IOCON-&amp;gt;P0_7 = 0x330;//CLK-&amp;gt;SPI&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_IOCON-&amp;gt;P0_8 = 0x330;//MISO-&amp;gt;SPI&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_IOCON-&amp;gt;P0_9 = 0x330;//MOSI-&amp;gt;GPIO&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;//LPC_GPIO0-&amp;gt;DIR &amp;amp;= ~(0x1&amp;lt;&amp;lt;8);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;//LPC_GPIO0-&amp;gt;DIR &amp;amp;= ~(0x1&amp;lt;&amp;lt;7);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;//LPC_GPIO0-&amp;gt;DIR &amp;amp;= ~(0x1&amp;lt;&amp;lt;9);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0-&amp;gt;DIR |= (0x1&amp;lt;&amp;lt;6);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0-&amp;gt;DIR |= (0x1&amp;lt;&amp;lt;8);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0-&amp;gt;DIR |= (0x1&amp;lt;&amp;lt;7);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0-&amp;gt;DIR |= (0x1&amp;lt;&amp;lt;9);&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;while (1)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // repeat forever&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;sprintf((char*)g_buf, "LPC_GPIO0 = %x\n\r", LPC_GPIO0-&amp;gt;PIN);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;DebugPuts(g_buf);&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;//if(LPC_GPIO0-&amp;gt;PIN &amp;amp; (1&amp;lt;&amp;lt;8))DebugPuts((uint8_t*)"High ...\n\r");&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;//elseDebugPuts((uint8_t*)"Low ...\n\r");&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0-&amp;gt;SET = 0x3C0;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;DelayMS(10000);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;sprintf((char*)g_buf, "LPC_GPIO0 = %x\n\r", LPC_GPIO0-&amp;gt;PIN);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;DebugPuts(g_buf);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0-&amp;gt;CLR = 0x3C0;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;DelayMS(10000);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;=====================================================================&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am getting like below.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0 = 7bfc07f&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0 = 7bfc03f&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0 = 7bfc07f&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0 = 7bfc03f&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0 = 7bfc07f&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0 = 7bfc03f&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0 = 7bfc07f&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0 = 7bfc03f&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0 = 7bfc07f&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0 = 7bfc03f&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0 = 7bfc07f&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0 = 7bfc03f&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Please let me the solution if anyone have.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:29:18 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:29:18Z</dc:date>
    <item>
      <title>LPC1788 144 pin QFP type: W-type IO having problem in input mode.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-144-pin-QFP-type-W-type-IO-having-problem-in-input-mode/m-p/517524#M2222</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by awadhesh on Thu Sep 04 04:06:41 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I want to interface micro SD card to ssp1 on pin 113, 112, 111, 109. But I had checked that problem in MISO pin i.e. 111(P0.8) not receiving anything from SD card. I checked it and there are data on that pin on oscilloscope.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Now I am going to check that&amp;nbsp; this pin can work in input mode or not. But it is always low whatever voltage applied on pin. After that I check the details of this pin, I got that these are W-type pin P0.7, P0.8, P0.9. I do same on all these pin, but these never read applied logic voltage.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;After I configured these as output and making these to high and low with some delays to blink four leds. All leds are blinking as per expectation. But when I read PIN register, only changing is in P0.6, which is D-type, all W-type cannot read these are always low, even connected leds are blinking. I configured these pins in every setting like-pull up, pull down, filter enable/disable, hys enable/disable etc, but never get result. code is here.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;========================================================================&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_IOCON-&amp;gt;P0_6 = 0x00;//SSEL-&amp;gt;SPI&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_IOCON-&amp;gt;P0_7 = 0x330;//CLK-&amp;gt;SPI&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_IOCON-&amp;gt;P0_8 = 0x330;//MISO-&amp;gt;SPI&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_IOCON-&amp;gt;P0_9 = 0x330;//MOSI-&amp;gt;GPIO&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;//LPC_GPIO0-&amp;gt;DIR &amp;amp;= ~(0x1&amp;lt;&amp;lt;8);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;//LPC_GPIO0-&amp;gt;DIR &amp;amp;= ~(0x1&amp;lt;&amp;lt;7);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;//LPC_GPIO0-&amp;gt;DIR &amp;amp;= ~(0x1&amp;lt;&amp;lt;9);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0-&amp;gt;DIR |= (0x1&amp;lt;&amp;lt;6);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0-&amp;gt;DIR |= (0x1&amp;lt;&amp;lt;8);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0-&amp;gt;DIR |= (0x1&amp;lt;&amp;lt;7);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0-&amp;gt;DIR |= (0x1&amp;lt;&amp;lt;9);&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;while (1)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // repeat forever&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;sprintf((char*)g_buf, "LPC_GPIO0 = %x\n\r", LPC_GPIO0-&amp;gt;PIN);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;DebugPuts(g_buf);&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;//if(LPC_GPIO0-&amp;gt;PIN &amp;amp; (1&amp;lt;&amp;lt;8))DebugPuts((uint8_t*)"High ...\n\r");&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;//elseDebugPuts((uint8_t*)"Low ...\n\r");&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0-&amp;gt;SET = 0x3C0;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;DelayMS(10000);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;sprintf((char*)g_buf, "LPC_GPIO0 = %x\n\r", LPC_GPIO0-&amp;gt;PIN);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;DebugPuts(g_buf);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0-&amp;gt;CLR = 0x3C0;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;DelayMS(10000);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;=====================================================================&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am getting like below.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0 = 7bfc07f&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0 = 7bfc03f&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0 = 7bfc07f&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0 = 7bfc03f&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0 = 7bfc07f&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0 = 7bfc03f&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0 = 7bfc07f&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0 = 7bfc03f&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0 = 7bfc07f&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0 = 7bfc03f&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0 = 7bfc07f&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_GPIO0 = 7bfc03f&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Please let me the solution if anyone have.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:29:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-144-pin-QFP-type-W-type-IO-having-problem-in-input-mode/m-p/517524#M2222</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:29:18Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1788 144 pin QFP type: W-type IO having problem in input mode.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-144-pin-QFP-type-W-type-IO-having-problem-in-input-mode/m-p/517525#M2223</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Pacman on Fri Sep 05 07:33:52 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The only difference between W and D pins is the filter function, as far as I can see.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Try setting P0_7, P0_8 and P0_9 to input and P0_0, P0_1 and P0_2 as output ...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; LPC_GPIO0-&amp;gt;DIR &amp;amp;= ~((1 &amp;lt;&amp;lt; 7) | (1 &amp;lt;&amp;lt; 8) | (1 &amp;lt;&amp;lt; 9));&amp;nbsp; /* P0[9:7] are inputs */
&amp;nbsp;&amp;nbsp;&amp;nbsp; LPC_GPIO0-&amp;gt;DIR |= (1 &amp;lt;&amp;lt; 0) | (1 &amp;lt;&amp;lt; 1) | (1 &amp;lt;&amp;lt; 2);&amp;nbsp; /* P0[2:0] are outputs */
&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;... then configure all 3 pins using the following value ...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; LPC_IOCON-&amp;gt;P0[7] = ((1 &amp;lt;&amp;lt; 5) | (1 &amp;lt;&amp;lt; 7));
&amp;nbsp;&amp;nbsp;&amp;nbsp; LPC_IOCON-&amp;gt;P0[8] = ((1 &amp;lt;&amp;lt; 5) | (1 &amp;lt;&amp;lt; 7));
&amp;nbsp;&amp;nbsp;&amp;nbsp; LPC_IOCON-&amp;gt;P0[9] = ((1 &amp;lt;&amp;lt; 5) | (1 &amp;lt;&amp;lt; 7));&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;... and read them and output them to each their own LED using ...&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; while(1)
&amp;nbsp;&amp;nbsp;&amp;nbsp; {
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; p0_7 = (LPC_GPIO0-&amp;gt;PIN &amp;gt;&amp;gt; 7) &amp;amp; 1;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; p0_8 = (LPC_GPIO0-&amp;gt;PIN &amp;gt;&amp;gt; 8) &amp;amp; 1;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; p0_9 = (LPC_GPIO0-&amp;gt;PIN &amp;gt;&amp;gt; 9) &amp;amp; 1;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; LPC_GPIO0-&amp;gt;PIN = (p0_7 &amp;lt;&amp;lt; 0) | (p0_8 &amp;lt;&amp;lt; 1) | (p0_9 &amp;lt;&amp;lt; 2);
&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The LEDs should connect on pin 66, 67 and 141. I recommend a 1K resistor from VCC to the LED's anode and then connect the LED's cathode to the pin on your LPC1788.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Now connect a 4K7 resistor to GND and the other end of the 4K7 resistor to a wire (I prefer single-strand).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;"probe" the wire on pin 109, 111 and 112 and see if there's any difference on the 3 LEDs.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Connect the 4K7 resistor to 3V3 instead and repeat the above action.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;(You can use any value between 1K and 10K for the 4K7 resistor; it's not important)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can you make any of the LEDs change by touching pin 109, 111 and 112 with the probe-wire ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:29:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-144-pin-QFP-type-W-type-IO-having-problem-in-input-mode/m-p/517525#M2223</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:29:19Z</dc:date>
    </item>
  </channel>
</rss>