<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC4357FET256 USB0 VBUS</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357FET256-USB0-VBUS/m-p/590758#M22115</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;bump&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 19 Jun 2016 01:03:51 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-19T01:03:51Z</dc:date>
    <item>
      <title>LPC4357FET256 USB0 VBUS</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357FET256-USB0-VBUS/m-p/590756#M22113</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by bpetty on Thu Mar 03 08:38:35 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I have run across some conflicting information and I need to track down the correct answer.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In the datasheet for the LPC4357FET256, page 57 lists the pin description for USB0_VBUS. It lists notes 6 and 7 for this pin. Note 6 on page 60 states: 5 V tolerant transparent analog pad.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;However, in the LPC4357FET256 User’s Manual, in Chapter 25 (USB0) and on page 644 is states: This input is only 5 V tolerant when VDDIO is present.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Which is correct? I need to know if the dedicate pin on the device, USB0_VBUS is 5V tolerant when power (VDDIO) is NOT present.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Many thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Brian&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:18:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357FET256-USB0-VBUS/m-p/590756#M22113</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:18:43Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4357FET256 USB0 VBUS</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357FET256-USB0-VBUS/m-p/590757#M22114</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by bavarian on Wed Mar 09 06:46:36 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The VBUS pin is only 5V tolerant when VDDIO is present. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In case of a bus powered device you need to add a protection, for example a simple AND picoGate device which only switches to '1' if VDDIO and VBUS are there. The resistor based voltage divider solution shown in the data sheet is a little bit tricky to use, so I don't recommend that.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;NXP Support Team&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:18:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357FET256-USB0-VBUS/m-p/590757#M22114</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:18:44Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4357FET256 USB0 VBUS</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357FET256-USB0-VBUS/m-p/590758#M22115</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;bump&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 19 Jun 2016 01:03:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357FET256-USB0-VBUS/m-p/590758#M22115</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-19T01:03:51Z</dc:date>
    </item>
  </channel>
</rss>