<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Clear backup registers by wakeup pin in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Clear-backup-registers-by-wakeup-pin/m-p/590420#M22061</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mtb98 on Tue Sep 30 05:57:57 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Using an LPC4357 development board and LPC4337 board see the same behavior.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Having problems getting the backup registers to clear with an event on the wakeup0 pin. Setup the event monitor with ERCONTRO set to 0xC000000A this enables GPCLEAR-EN0 and EV0-INPUT_EN and set sample clock to 1Khz.&amp;nbsp; Take the wakeup0 pin from low to high and see ERSTATUS go to 0x00000009 with GP-CLEARED and EV0 set. Also the ERCOUNTER increments for COUNTER0, and I get timestamps for the event.&amp;nbsp; But when I look at the backup registers (REGFILE) they are not cleared they contain same values as before the wakeup0 pin was cycled.&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Am I missing a register I need to configure? &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:17:38 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:17:38Z</dc:date>
    <item>
      <title>Clear backup registers by wakeup pin</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Clear-backup-registers-by-wakeup-pin/m-p/590420#M22061</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mtb98 on Tue Sep 30 05:57:57 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Using an LPC4357 development board and LPC4337 board see the same behavior.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Having problems getting the backup registers to clear with an event on the wakeup0 pin. Setup the event monitor with ERCONTRO set to 0xC000000A this enables GPCLEAR-EN0 and EV0-INPUT_EN and set sample clock to 1Khz.&amp;nbsp; Take the wakeup0 pin from low to high and see ERSTATUS go to 0x00000009 with GP-CLEARED and EV0 set. Also the ERCOUNTER increments for COUNTER0, and I get timestamps for the event.&amp;nbsp; But when I look at the backup registers (REGFILE) they are not cleared they contain same values as before the wakeup0 pin was cycled.&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Am I missing a register I need to configure? &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:17:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Clear-backup-registers-by-wakeup-pin/m-p/590420#M22061</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:17:38Z</dc:date>
    </item>
  </channel>
</rss>