<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SGPIO + parallel interface in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/SGPIO-parallel-interface/m-p/590388#M22060</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I try a similar thing.&lt;BR /&gt;The output of parallel data 8bit and clk 1bit&lt;BR /&gt;Please tell me the register setting if I work well&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 Oct 2016 06:20:19 GMT</pubDate>
    <dc:creator>atsuyosano</dc:creator>
    <dc:date>2016-10-17T06:20:19Z</dc:date>
    <item>
      <title>SGPIO + parallel interface</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SGPIO-parallel-interface/m-p/590386#M22058</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by JMRouxel on Tue Jan 06 01:19:40 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm working on the LP4350 part. I'm trying to use SGPIO to configure FPGA with parallel 8-bits data. It's the first time I try to use SGPIO and it seems a little confused for me for the moment.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So, to begin with SGPIO, I'm starting my tests from the following example : SGPIO_spi_master from the library lpc43xx.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;This example emulates a SPI master (CLK, CS, MISO and MOSI). I can see the different signals on a scope (the clock for example).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;My goal is to change the MOSI signal data (which is using just a SGPIO) to a parallel 8-bits data (with the use of 8 SGPIO)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;First, when I modify the bits PARALLEL_MODE of the SLICE_MUX_CFG register (shift 1 bit per clock -&amp;gt; 1 byte per clock), I can't see the clock on my scope any more.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I assume that other parameters must be changed, but which?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can anyone help me?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:17:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SGPIO-parallel-interface/m-p/590386#M22058</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:17:23Z</dc:date>
    </item>
    <item>
      <title>Re: SGPIO + parallel interface</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SGPIO-parallel-interface/m-p/590387#M22059</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by JohnR on Thu Jan 08 07:47:59 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;There is an SGPIO example that may be closer to what you are doing.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;AN11343 SGPIO camera module design using LPC4300&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;From the text &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: &lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;The OV7670 is controlled via an I2C interface taking commands from LPC4300. Its output is a byte wide interface that sends out one byte per pixel clock. As each pixel is represented by 16 bits of data in an RGB565 format, it takes 2 pixel clocks from the camera to send out one pixel of image data&lt;BR /&gt;&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I hope this helps&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;JohnR&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:17:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SGPIO-parallel-interface/m-p/590387#M22059</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:17:24Z</dc:date>
    </item>
    <item>
      <title>Re: SGPIO + parallel interface</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SGPIO-parallel-interface/m-p/590388#M22060</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I try a similar thing.&lt;BR /&gt;The output of parallel data 8bit and clk 1bit&lt;BR /&gt;Please tell me the register setting if I work well&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Oct 2016 06:20:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SGPIO-parallel-interface/m-p/590388#M22060</guid>
      <dc:creator>atsuyosano</dc:creator>
      <dc:date>2016-10-17T06:20:19Z</dc:date>
    </item>
  </channel>
</rss>