<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: micro SD over SGPIO?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/micro-SD-over-SGPIO/m-p/589682#M21976</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by wmues on Mon Jan 14 03:42:15 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;MicroSD is the same interface as normal SD. No difference.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;You can make an interface with SPI, or use the SD mode.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In SD mode, you will have to check for a leading "0" bit in the responses from the SD card (like a V24).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;And: you will have to implement CRC. CRC is calculated per IO line. If you have a 4bit interface, you will need to calculate 4 CRC values.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:16:31 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:16:31Z</dc:date>
    <item>
      <title>micro SD over SGPIO?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/micro-SD-over-SGPIO/m-p/589681#M21975</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by tomkulaga on Mon Jan 14 02:56:30 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I was wondering if anyone has done it or if it is even feasible to create and micro Sd interface through the SGPIO on the lpc4330?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Tom&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:16:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/micro-SD-over-SGPIO/m-p/589681#M21975</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:16:30Z</dc:date>
    </item>
    <item>
      <title>Re: micro SD over SGPIO?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/micro-SD-over-SGPIO/m-p/589682#M21976</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by wmues on Mon Jan 14 03:42:15 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;MicroSD is the same interface as normal SD. No difference.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;You can make an interface with SPI, or use the SD mode.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In SD mode, you will have to check for a leading "0" bit in the responses from the SD card (like a V24).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;And: you will have to implement CRC. CRC is calculated per IO line. If you have a 4bit interface, you will need to calculate 4 CRC values.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:16:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/micro-SD-over-SGPIO/m-p/589682#M21976</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:16:31Z</dc:date>
    </item>
  </channel>
</rss>