<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC1769 and voltage divider for USB VBUS</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-and-voltage-divider-for-USB-VBUS/m-p/517456#M2194</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by robert hulsebos on Thu Dec 17 05:37:03 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for your response!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I understand reason behind the voltage divider. The thing is we use the USB function in self-powered design and only recently found out that the voltage divider is recommended. At the time of our original design there was no voltage divider in the NXP documentation... I asked the questions because I am unsure as to we should do a redesign of the PCB for including the voltage divider, or if we could continue to use the existing PCB design without the voltage divider. With acceptable risk. I hope somebody from NXP can elaborate on the risks involved so I can make a decision...&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:27:58 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:27:58Z</dc:date>
    <item>
      <title>LPC1769 and voltage divider for USB VBUS</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-and-voltage-divider-for-USB-VBUS/m-p/517453#M2191</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by robert hulsebos on Fri Dec 11 09:04:49 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi all,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;We have a PCB that uses the LCP1769 and configures its USB port as an USB device. It is a self-powered design, the LPC1769 does not derive its power from the USB bus. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In more recent versions of the LPC176x datasheet / AN11392 it is recommended that two resistors are added to the VBUS signal of the USB port. These resistors are to function as a voltage-divider for bringing down the 5V of the VBUS signal to the maximum allowed 3.6V. (see paragraph 5.1 of most recent datasheet) &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;As our PCB design predates these recommendations, it does not include the voltage-divider. However, it does include a series resistor of 1K in the line to the VBUS pin.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;My questions now are:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;1. Is VBUS voltage-divider really required ? What is the real risk of not having the voltage-divider ? &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2. Is the 1K series resistor a sufficient means of mitigating this risk ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;3. What are the recommended values for the resistors of the voltage-divider ? &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I noticed in other forums on this site that for other LPC families NXP recommendations are [u]not[/u] to use a voltage-divider, but other circuity instead.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;SPAN&gt;( e.g. see &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.lpcware.com%2Fcontent%2Fforum%2Fusb0-vbus-voltage-divider" rel="nofollow" target="_blank"&gt;https://www.lpcware.com/content/forum/usb0-vbus-voltage-divider&lt;/A&gt;&lt;SPAN&gt; ) &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;3. Does this now also apply for the LPC1769 - has NXP insight on this matter changed?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Robert&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:27:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-and-voltage-divider-for-USB-VBUS/m-p/517453#M2191</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:27:56Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1769 and voltage divider for USB VBUS</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-and-voltage-divider-for-USB-VBUS/m-p/517454#M2192</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by masaz on Mon Dec 14 05:23:16 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have had the understanding that while most I/O pins are 5V tolerant, this applies&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;only when the device is powered up, while in USB self powered design, the&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;device can be connected to USB without power. Thus, it is suggested to use the&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;voltage divider.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In addition, the same pin can be used to analog function (ADC) which is never&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;5 V tolerant.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Br, Matti&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:27:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-and-voltage-divider-for-USB-VBUS/m-p/517454#M2192</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:27:56Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1769 and voltage divider for USB VBUS</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-and-voltage-divider-for-USB-VBUS/m-p/517455#M2193</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by masaz on Mon Dec 14 05:32:15 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;NXP USB application note suggests 24k to VBUS and 39k to ground, input from between. I have used 4.7k and 10k.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;See:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fdocuments%2Fapplication_note%2FAN11392.pdf" rel="nofollow" target="_blank"&gt;http://www.nxp.com/documents/application_note/AN11392.pdf&lt;/A&gt;&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:27:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-and-voltage-divider-for-USB-VBUS/m-p/517455#M2193</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:27:57Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1769 and voltage divider for USB VBUS</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-and-voltage-divider-for-USB-VBUS/m-p/517456#M2194</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by robert hulsebos on Thu Dec 17 05:37:03 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for your response!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I understand reason behind the voltage divider. The thing is we use the USB function in self-powered design and only recently found out that the voltage divider is recommended. At the time of our original design there was no voltage divider in the NXP documentation... I asked the questions because I am unsure as to we should do a redesign of the PCB for including the voltage divider, or if we could continue to use the existing PCB design without the voltage divider. With acceptable risk. I hope somebody from NXP can elaborate on the risks involved so I can make a decision...&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:27:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-and-voltage-divider-for-USB-VBUS/m-p/517456#M2194</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:27:58Z</dc:date>
    </item>
  </channel>
</rss>