<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: farnell lpc4357 eva board in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/farnell-lpc4357-eva-board/m-p/589153#M21899</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by bavarian on Thu Feb 07 10:53:41 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The settings in your screenshots look mainly fine, but you should select as target the LPC4357 instead of LPC4350.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Then you get the correct memory sizes automatically (LPC4357 has less SRAM than LPC4350)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;For an image in internal flash you also need to generate signature which is added to the image.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In the User tab (Run user command after Build/Rebuild) you need to add the following command:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;$K\ARM\BIN\ELFDWT.EXE !L BASEADDRESS(0x1A000000)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This generates and appends the correct signature for flash bank #A&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Then you need to load the correct flash algorithm in Utilities tab (Settings --&amp;gt; Add --&amp;gt; LPC18xx/43xx IAP 512kB Flash Bank A)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Hope this helps.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:13:11 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:13:11Z</dc:date>
    <item>
      <title>farnell lpc4357 eva board</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/farnell-lpc4357-eva-board/m-p/589151#M21897</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lgeorge123 on Thu Feb 07 07:37:13 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;In farnell lpc4357 eva board with lcd it supplied EMWIN GUI demo example , but it only provided external flash method only , can someone upload in flash whole keil folder as I transplant to ledblinkly led example folder it give out insufficient space , the compiler error is shows as attached picture ....&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:13:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/farnell-lpc4357-eva-board/m-p/589151#M21897</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:13:10Z</dc:date>
    </item>
    <item>
      <title>Re: farnell lpc4357 eva board</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/farnell-lpc4357-eva-board/m-p/589152#M21898</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lgeorge123 on Thu Feb 07 07:39:17 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I also upload another picture .....&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:13:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/farnell-lpc4357-eva-board/m-p/589152#M21898</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:13:10Z</dc:date>
    </item>
    <item>
      <title>Re: farnell lpc4357 eva board</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/farnell-lpc4357-eva-board/m-p/589153#M21899</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by bavarian on Thu Feb 07 10:53:41 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The settings in your screenshots look mainly fine, but you should select as target the LPC4357 instead of LPC4350.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Then you get the correct memory sizes automatically (LPC4357 has less SRAM than LPC4350)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;For an image in internal flash you also need to generate signature which is added to the image.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In the User tab (Run user command after Build/Rebuild) you need to add the following command:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;$K\ARM\BIN\ELFDWT.EXE !L BASEADDRESS(0x1A000000)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This generates and appends the correct signature for flash bank #A&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Then you need to load the correct flash algorithm in Utilities tab (Settings --&amp;gt; Add --&amp;gt; LPC18xx/43xx IAP 512kB Flash Bank A)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Hope this helps.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:13:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/farnell-lpc4357-eva-board/m-p/589153#M21899</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:13:11Z</dc:date>
    </item>
  </channel>
</rss>