<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC4330 Xplorer Boot from USB0 not working in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4330-Xplorer-Boot-from-USB0-not-working/m-p/588967#M21874</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by joohyun.seo on Tue Aug 26 14:05:24 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.lpcware.com%2Fcontent%2Fforum%2Fprogramming-mcb4300-usb0" rel="nofollow" target="_blank"&gt;http://www.lpcware.com/content/forum/programming-mcb4300-usb0&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;This helps me solve the problem. Now, I can see that in DFU programmer it displays High Speed USB.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:18:13 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:18:13Z</dc:date>
    <item>
      <title>LPC4330 Xplorer Boot from USB0 not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4330-Xplorer-Boot-from-USB0-not-working/m-p/588966#M21873</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by joohyun.seo on Tue Aug 26 13:45:32 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi All,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have a LPC4330 Xplorer evaluation board, and I am trying to boot from USB0 following the instruction :&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.lpcware.com%2Fcontent%2Fproject%2Fdfu-download-programming-utility-and-security-lpcdfusec-tool" rel="nofollow" target="_blank"&gt;http://www.lpcware.com/content/project/dfu-download-programming-utility-and-security-lpcdfusec-tool&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The problem is that when I plugged the USB cable into USB0 port, I cannot see any change in the device manager in my Win7 64-bit machine. Of course, in DFU programmer, the status is displayed as 'NO CONN'.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have utilized the evaluation board using various examples in LPCOpen_2.12, and now I configured the boot source switch such that (P2_9, P2_8, P1_2, P1_1) to be (Low, High, Low, High) as directed for USB0 boot mode. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Currently, if I connect both USB0, USB1 ports, then the connection through USB1 port is acknowledged as communication port, because I install that VCOM driver for initial peripheral test, but USB0 is not acknowledged by my machine at all. However, when I perform the peripheral test by pressing a switch on the board, then USB0 port is acknowledged because in the middle of the peripheral test, there is a USB0 enumeration as a HID device. Thus, I guess USB0 can still make a connection to the PC.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;However, I initially thought that USB0 should be at least acknowledged by the PC once it is connected, but since it doesn't appear in the device manager, I can't even install the WINUSB driver.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Could anyone help me or guide me to solve this issue?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Many thanks in advance.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:18:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4330-Xplorer-Boot-from-USB0-not-working/m-p/588966#M21873</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:18:12Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4330 Xplorer Boot from USB0 not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4330-Xplorer-Boot-from-USB0-not-working/m-p/588967#M21874</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by joohyun.seo on Tue Aug 26 14:05:24 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.lpcware.com%2Fcontent%2Fforum%2Fprogramming-mcb4300-usb0" rel="nofollow" target="_blank"&gt;http://www.lpcware.com/content/forum/programming-mcb4300-usb0&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;This helps me solve the problem. Now, I can see that in DFU programmer it displays High Speed USB.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:18:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4330-Xplorer-Boot-from-USB0-not-working/m-p/588967#M21874</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:18:13Z</dc:date>
    </item>
  </channel>
</rss>