<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SDRAM A0 is too slow. What might be the problem? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/SDRAM-A0-is-too-slow-What-might-be-the-problem/m-p/588907#M21869</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In addition to this Bank select are not doing anything and CAS+RAS are at 3.3V at all times.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Aug 2016 13:15:02 GMT</pubDate>
    <dc:creator>moller</dc:creator>
    <dc:date>2016-08-10T13:15:02Z</dc:date>
    <item>
      <title>SDRAM A0 is too slow. What might be the problem?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SDRAM-A0-is-too-slow-What-might-be-the-problem/m-p/588906#M21868</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to configure my AS4C2M32SA-6TIN 64MB SDRAM on my LPC4337 (costum board). &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have verified that the EMC clock is half M4 core clock (204/2=102MHz) but when measuring A0&lt;BR /&gt;this is only running at 1MHz (expected to run at half core clock when read/write to the entire SDRAM).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What could be the reason for this? I got an MPC4357-EVB with 32MB 16-bit SDRAM and got the example working in uVision.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When trying to use this example on my 64MB 32-bit SDRAM in emIDE (with corrected parameters that fits this SDRAM) nothing works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;my config setup can be seen here &lt;A href="http://pastebin.com/WAu4hXke" title="http://pastebin.com/WAu4hXke"&gt;http://pastebin.com/WAu4hXke&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope someone is able to help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Aug 2016 08:08:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SDRAM-A0-is-too-slow-What-might-be-the-problem/m-p/588906#M21868</guid>
      <dc:creator>moller</dc:creator>
      <dc:date>2016-08-10T08:08:47Z</dc:date>
    </item>
    <item>
      <title>Re: SDRAM A0 is too slow. What might be the problem?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SDRAM-A0-is-too-slow-What-might-be-the-problem/m-p/588907#M21869</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In addition to this Bank select are not doing anything and CAS+RAS are at 3.3V at all times.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Aug 2016 13:15:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SDRAM-A0-is-too-slow-What-might-be-the-problem/m-p/588907#M21869</guid>
      <dc:creator>moller</dc:creator>
      <dc:date>2016-08-10T13:15:02Z</dc:date>
    </item>
  </channel>
</rss>