<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Is it possible to communicate with more than one Device using TCP/IP communication through LPC1768 Based  controller Board??? in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Is-it-possible-to-communicate-with-more-than-one-Device-using/m-p/588347#M21791</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is possible, however we don´t have an example like you need however you can check the below threads as reference:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://developer.mbed.org/questions/1492/Cant-get-more-than-3-active-TCP-connecti/" title="https://developer.mbed.org/questions/1492/Cant-get-more-than-3-active-TCP-connecti/"&gt;Can't get more than 3 active TCP connections - Question | mbed&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://developer.mbed.org/forum/mbed/topic/3741/" title="https://developer.mbed.org/forum/mbed/topic/3741/"&gt;EthernetInterface Library | mbed&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 27 Dec 2016 17:32:03 GMT</pubDate>
    <dc:creator>soledad</dc:creator>
    <dc:date>2016-12-27T17:32:03Z</dc:date>
    <item>
      <title>Is it possible to communicate with more than one Device using TCP/IP communication through LPC1768 Based  controller Board???</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Is-it-possible-to-communicate-with-more-than-one-Device-using/m-p/588346#M21790</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;STRONG&gt;&lt;EM&gt;I would like to get excuse from all of you before Explaining my issue. It may look so simple for you all. But as I am new to the world of Ethernet communication using controllers no other option for me to get solution rather than this.&lt;/EM&gt;&lt;/STRONG&gt; &lt;/P&gt;&lt;P&gt;We are using an&lt;STRONG&gt; LPC1768&lt;/STRONG&gt; Based controller Board with a Ethernet Port. &lt;STRONG&gt;LPCXpresso&lt;/STRONG&gt; is the IDE we are working with. I am working with TCP/IP protocol right now. I am looking for a solution to my problem.&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;The controller is used to communicate with A camera and one more Device, All the 3 in the Same network.&lt;/LI&gt;&lt;LI&gt;Both Based on TCP/IP protocol. &lt;/LI&gt;&lt;LI&gt;I have to send few commands for controlling the functionality of both through TCP/IP as&amp;nbsp; I mentioned earlier. Few commands will Reply with some data's (A two way communication is requires were Controller Board acting as Master and both Devices as Slave)&lt;/LI&gt;&lt;LI&gt;Using&lt;STRONG&gt; Easyweb&lt;/STRONG&gt; Library I could communicate with one at a time&lt;/LI&gt;&lt;LI&gt;I cant give Dedicated Boards to control&amp;nbsp; them separately.&lt;/LI&gt;&lt;LI&gt;I need some one to Help me to come out from the issue.&lt;/LI&gt;&lt;LI&gt;Suggest a Library for my Requirement which can send data to 2 different IP address Devices.&lt;/LI&gt;&lt;LI&gt;I should be able to address two devices and I have to get connected with both devices for Sending and Receiving Packets&lt;/LI&gt;&lt;LI&gt;If the controller we use have any limitations Suggest me a better option to achieve my Goal&lt;/LI&gt;&lt;LI&gt;Thank you all in advance. ! &lt;/LI&gt;&lt;/OL&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Aug 2016 07:44:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Is-it-possible-to-communicate-with-more-than-one-Device-using/m-p/588346#M21790</guid>
      <dc:creator>chithraks</dc:creator>
      <dc:date>2016-08-10T07:44:11Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to communicate with more than one Device using TCP/IP communication through LPC1768 Based  controller Board???</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Is-it-possible-to-communicate-with-more-than-one-Device-using/m-p/588347#M21791</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is possible, however we don´t have an example like you need however you can check the below threads as reference:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://developer.mbed.org/questions/1492/Cant-get-more-than-3-active-TCP-connecti/" title="https://developer.mbed.org/questions/1492/Cant-get-more-than-3-active-TCP-connecti/"&gt;Can't get more than 3 active TCP connections - Question | mbed&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://developer.mbed.org/forum/mbed/topic/3741/" title="https://developer.mbed.org/forum/mbed/topic/3741/"&gt;EthernetInterface Library | mbed&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Dec 2016 17:32:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Is-it-possible-to-communicate-with-more-than-one-Device-using/m-p/588347#M21791</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2016-12-27T17:32:03Z</dc:date>
    </item>
  </channel>
</rss>