<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: SDRAM AND SDCARD TOGETHER ?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/SDRAM-AND-SDCARD-TOGETHER/m-p/587707#M21683</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by manes6969 on Wed May 08 11:16:27 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;&amp;lt;em&amp;gt;Found the answer !&amp;lt;/em&amp;gt;&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;pin pc0 is also a pin which has a sdio_clk function. Unfortunately this pin is used for lcd (not connected so far).&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;On the keil mcb4357 board its connected that way ...&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;maybe i can cut a wire and connect pc0 as clk for the sdio.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Greetings Ronny&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;lt;em&amp;gt;&lt;BR /&gt;&amp;lt;/em&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:13:17 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:13:17Z</dc:date>
    <item>
      <title>SDRAM AND SDCARD TOGETHER ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SDRAM-AND-SDCARD-TOGETHER/m-p/587706#M21682</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by manes6969 on Wed May 08 10:37:32 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;I have succesfully setup the sdram controller to work on the lpc4357 evb from element14. Now i'm trying to get the sdio at work.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;The clk for the sdcard is sfclk2. But on this forum I read that all 4 emc clocks are needed for the sdram. And indeed if I use 1 or more clocks for something else like the sdram , then my memory test fails.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;So my question , how do you use sdram and sdio at the same time , if all 4 clocks seem to be needed for emc ?&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Hoping someone can help me on this&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Ronny&lt;/P&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:13:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SDRAM-AND-SDCARD-TOGETHER/m-p/587706#M21682</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:13:16Z</dc:date>
    </item>
    <item>
      <title>Re: SDRAM AND SDCARD TOGETHER ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SDRAM-AND-SDCARD-TOGETHER/m-p/587707#M21683</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by manes6969 on Wed May 08 11:16:27 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;&amp;lt;em&amp;gt;Found the answer !&amp;lt;/em&amp;gt;&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;pin pc0 is also a pin which has a sdio_clk function. Unfortunately this pin is used for lcd (not connected so far).&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;On the keil mcb4357 board its connected that way ...&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;maybe i can cut a wire and connect pc0 as clk for the sdio.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Greetings Ronny&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;lt;em&amp;gt;&lt;BR /&gt;&amp;lt;/em&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:13:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SDRAM-AND-SDCARD-TOGETHER/m-p/587707#M21683</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:13:17Z</dc:date>
    </item>
    <item>
      <title>Re: SDRAM AND SDCARD TOGETHER ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SDRAM-AND-SDCARD-TOGETHER/m-p/587708#M21684</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Hydron on Wed May 08 17:54:42 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;You may be able to assign two emc clocks to one pin, to reduce the pins needed from 4 to 2. If you look in the docs, there are two emc clock pins which can be configured as clock 01 and clock 23, I believe if you use them in this configuration it meets the requirements of having all four clocks enabled. Its a weird and annoying design, we spent a lot of time trying to get the ram going before we realised this :(&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:13:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SDRAM-AND-SDCARD-TOGETHER/m-p/587708#M21684</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:13:18Z</dc:date>
    </item>
    <item>
      <title>Re: SDRAM AND SDCARD TOGETHER ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SDRAM-AND-SDCARD-TOGETHER/m-p/587709#M21685</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by kjschaefer on Tue Jul 08 07:02:54 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The SD slot on the LPC4357-EVB is useless if the LCD or the SDRAM is in operation:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;According to the user manual (UM10503.pdf page 578) all four CLKn outputs need to be configured to mode 0 if a SDRAM is used. So the &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;SD_CLK option for CLK2 can not be used.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The only other option to get the SDIO CLK signal would be Port C pin 0.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;But this one is wired to the LCD (LCD_DCLK).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;-&amp;gt; No way :-(&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:13:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SDRAM-AND-SDCARD-TOGETHER/m-p/587709#M21685</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:13:18Z</dc:date>
    </item>
  </channel>
</rss>