<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックPossible error in pin assignment for LPC4370</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Possible-error-in-pin-assignment-for-LPC4370/m-p/585893#M21333</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by JohnR on Tue Mar 18 09:32:42 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I think there might some errors in board.c&amp;nbsp; for the lpc_board_nxp_lpclink2_4370 package&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In Board_SSP_Init(LPC_SSP_T *pSSP)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;[codeelse if (pSSP == LPC_SSP1) {&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/* Set up clock and muxing for SSP1 interface */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/* P1.19 connected to SCL/SCLKSCU_MODE_FUNC1=SSP1 SCK1 */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Chip_SCU_PinMuxSet(0xF, 4, (SCU_PINIO_FAST | SCU_MODE_FUNC1)); // was (0x1, 19,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;///* P1.20 connected to nCSSCU_MODE_FUNC1=SSP1 SSEL1 */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;//Chip_SCU_PinMuxSet(0x1, 20, (SCU_PINIO_FAST | SCU_MODE_FUNC1));&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/* P0.0 connected to SOSCU_MODE_FUNC1=SSP1 MISO1 */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Chip_SCU_PinMuxSet(0x1, 3, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_FUNC1)); // was 0x0, 0,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/* P0.1 connected to nSISCU_MODE_FUNC2=SSP1 MOSI1 */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Chip_SCU_PinMuxSet(0x1, 4, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_FUNC1)); // was 0x0, 1&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;][/code]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt; I think the original values maybe are for the Hitex boards not the Link 2 card?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The chip select is set to a regular output configuration.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;JohnR.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 20:26:49 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T20:26:49Z</dc:date>
    <item>
      <title>Possible error in pin assignment for LPC4370</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Possible-error-in-pin-assignment-for-LPC4370/m-p/585893#M21333</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by JohnR on Tue Mar 18 09:32:42 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I think there might some errors in board.c&amp;nbsp; for the lpc_board_nxp_lpclink2_4370 package&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In Board_SSP_Init(LPC_SSP_T *pSSP)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;[codeelse if (pSSP == LPC_SSP1) {&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/* Set up clock and muxing for SSP1 interface */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/* P1.19 connected to SCL/SCLKSCU_MODE_FUNC1=SSP1 SCK1 */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Chip_SCU_PinMuxSet(0xF, 4, (SCU_PINIO_FAST | SCU_MODE_FUNC1)); // was (0x1, 19,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;///* P1.20 connected to nCSSCU_MODE_FUNC1=SSP1 SSEL1 */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;//Chip_SCU_PinMuxSet(0x1, 20, (SCU_PINIO_FAST | SCU_MODE_FUNC1));&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/* P0.0 connected to SOSCU_MODE_FUNC1=SSP1 MISO1 */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Chip_SCU_PinMuxSet(0x1, 3, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_FUNC1)); // was 0x0, 0,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;/* P0.1 connected to nSISCU_MODE_FUNC2=SSP1 MOSI1 */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Chip_SCU_PinMuxSet(0x1, 4, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_FUNC1)); // was 0x0, 1&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;][/code]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt; I think the original values maybe are for the Hitex boards not the Link 2 card?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The chip select is set to a regular output configuration.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;JohnR.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:26:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Possible-error-in-pin-assignment-for-LPC4370/m-p/585893#M21333</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:26:49Z</dc:date>
    </item>
    <item>
      <title>Re: Possible error in pin assignment for LPC4370</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Possible-error-in-pin-assignment-for-LPC4370/m-p/585894#M21334</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by sundarapandian on Thu Mar 20 15:46:41 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you for pointing it out. To use SSP1 via Serial expansion connector J3, please use the following Pin Mux configuration code&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;
if (pSSP == LPC_SSP1) {
/* SSEL: P1.20: J3 PIN-6 [Serial Expansion Interface] */
Chip_SCU_PinMuxSet(0x1, 20, (SCU_PINIO_FAST | SCU_MODE_FUNC1));
/* MISO: P1.3: J3 PIN-5 [Serial Expansion Interface] */
Chip_SCU_PinMuxSet(0x1, 3, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_FUNC5));
/* MOSI: P1.4: J3 PIN-4 [Serial Expansion Interface] */
Chip_SCU_PinMuxSet(0x1, 4, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_FUNC5));
/* SCLK: PF.4: J3 PIN-3 [Serial Expansion Interface] */
Chip_SCU_PinMuxSet(0xF, 4, (SCU_PINIO_FAST | SCU_MODE_FUNC0));
}
&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;This will be a part of the next release.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:26:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Possible-error-in-pin-assignment-for-LPC4370/m-p/585894#M21334</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:26:50Z</dc:date>
    </item>
  </channel>
</rss>