<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: lcd resolution problem in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/lcd-resolution-problem/m-p/517303#M2132</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Pacman on Tue Mar 11 06:23:55 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;You're probably setting it to a 4-bit-per-pixel resolution.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;That means... writing a single byte to an address in the screen area will change two pixels at the same time.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:27:39 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:27:39Z</dc:date>
    <item>
      <title>lcd resolution problem</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lcd-resolution-problem/m-p/517302#M2131</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jalila211 on Fri Feb 21 07:17:31 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;hi&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;i design a board with lpc1788 and use lcd controller for driving 15" lcd in 1024*768 resolution. by modifying CMSIS library example i can drive this lcd in 320*240 and every thing is ok. but when i change the setting to make higher resolution like 640*480 my logo image is not showed correctly. although the cursor is showed ok. in memory windows i set the one pixel color manually to red and seen that two pixel showed in screen! can any body help me?&lt;/SPAN&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337926"&gt;code.rar&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:27:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lcd-resolution-problem/m-p/517302#M2131</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:27:39Z</dc:date>
    </item>
    <item>
      <title>Re: lcd resolution problem</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lcd-resolution-problem/m-p/517303#M2132</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Pacman on Tue Mar 11 06:23:55 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;You're probably setting it to a 4-bit-per-pixel resolution.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;That means... writing a single byte to an address in the screen area will change two pixels at the same time.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:27:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lcd-resolution-problem/m-p/517303#M2132</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:27:39Z</dc:date>
    </item>
  </channel>
</rss>