<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックGPIO Pin interrupt issue</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/GPIO-Pin-interrupt-issue/m-p/585549#M21277</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by suhel on Thu May 29 22:31:29 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;i am working with LPC4370, and i am using two GPIO pin interrupts, Pin_Int0_IRQ and&amp;nbsp; Pin_Int1_IRQ, i have configured them as edge sensitive (rising edge), but the issue is even though i connect the input to ground, it fires an interrupt, continously as long as it is connected. if i leave it floating there is no interrupt.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;form the GPIO input pins i tried Pulling them down&amp;nbsp; as well as both pull up and pull down disabled.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;can any one point out where i might be going wrong.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Suhel&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 20:26:19 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T20:26:19Z</dc:date>
    <item>
      <title>GPIO Pin interrupt issue</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/GPIO-Pin-interrupt-issue/m-p/585549#M21277</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by suhel on Thu May 29 22:31:29 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;i am working with LPC4370, and i am using two GPIO pin interrupts, Pin_Int0_IRQ and&amp;nbsp; Pin_Int1_IRQ, i have configured them as edge sensitive (rising edge), but the issue is even though i connect the input to ground, it fires an interrupt, continously as long as it is connected. if i leave it floating there is no interrupt.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;form the GPIO input pins i tried Pulling them down&amp;nbsp; as well as both pull up and pull down disabled.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;can any one point out where i might be going wrong.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Suhel&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:26:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/GPIO-Pin-interrupt-issue/m-p/585549#M21277</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:26:19Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO Pin interrupt issue</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/GPIO-Pin-interrupt-issue/m-p/585550#M21278</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by rocketdawg on Fri May 30 08:55:37 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;we will have to see the pin setup code and the ISR code.&amp;nbsp; Otherwise you will have to provide a crystal ball we can gaze into.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:26:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/GPIO-Pin-interrupt-issue/m-p/585550#M21278</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:26:20Z</dc:date>
    </item>
  </channel>
</rss>