<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックHelp me choose: SSP or SGPIO</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Help-me-choose-SSP-or-SGPIO/m-p/585111#M21173</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mark03 on Mon Oct 22 17:54:28 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm interfacing a serial A/D (LTC237x series) to an LPC4357, and trying to decide the optimal solution for having the data transfer "in the background" as much as possible.&amp;nbsp; Ideally I would like the data to fill a DMA buffer in RAM without spending any CPU cycles until the buffer needs emptying.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I will drive the A/D conversion clock with a GPIO timer/counter output.&amp;nbsp; The A/D indicates it is done by the falling edge of a BUSY signal, and requires the host to provide SCLK and read the bits back.&amp;nbsp; Based on my reading of the LPC user's guide, if I use SSP the only way I can perform a read is to write dummy words.&amp;nbsp; The SSP has a nice FIFO, which would probably suffice in place of a DMA buffer, IF I could have that FIFO filling autonomously, but it's not clear to me that this is possible.&amp;nbsp; I can't just load up the transmit FIFO, then sit back and wait, because the SSP must only transmit/receive a frame when an A/D sample is ready.&amp;nbsp; I don't see any way to achieve this without CPU involvement (interrupt based).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Not really liking that prospect, I was looking at SGPIO.&amp;nbsp; There's no sample FIFO there (only the bit FIFOs for deserialization), so I would want to use DMA.&amp;nbsp; The user's guide says this is possible, but has anyone actually tried it [successfully]?&amp;nbsp; I'd feel a lot better with a working example to look at.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any other suggestions?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Mark&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:11:01 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:11:01Z</dc:date>
    <item>
      <title>Help me choose: SSP or SGPIO</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Help-me-choose-SSP-or-SGPIO/m-p/585111#M21173</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mark03 on Mon Oct 22 17:54:28 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm interfacing a serial A/D (LTC237x series) to an LPC4357, and trying to decide the optimal solution for having the data transfer "in the background" as much as possible.&amp;nbsp; Ideally I would like the data to fill a DMA buffer in RAM without spending any CPU cycles until the buffer needs emptying.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I will drive the A/D conversion clock with a GPIO timer/counter output.&amp;nbsp; The A/D indicates it is done by the falling edge of a BUSY signal, and requires the host to provide SCLK and read the bits back.&amp;nbsp; Based on my reading of the LPC user's guide, if I use SSP the only way I can perform a read is to write dummy words.&amp;nbsp; The SSP has a nice FIFO, which would probably suffice in place of a DMA buffer, IF I could have that FIFO filling autonomously, but it's not clear to me that this is possible.&amp;nbsp; I can't just load up the transmit FIFO, then sit back and wait, because the SSP must only transmit/receive a frame when an A/D sample is ready.&amp;nbsp; I don't see any way to achieve this without CPU involvement (interrupt based).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Not really liking that prospect, I was looking at SGPIO.&amp;nbsp; There's no sample FIFO there (only the bit FIFOs for deserialization), so I would want to use DMA.&amp;nbsp; The user's guide says this is possible, but has anyone actually tried it [successfully]?&amp;nbsp; I'd feel a lot better with a working example to look at.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any other suggestions?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Mark&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:11:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Help-me-choose-SSP-or-SGPIO/m-p/585111#M21173</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:11:01Z</dc:date>
    </item>
    <item>
      <title>Re: Help me choose: SSP or SGPIO</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Help-me-choose-SSP-or-SGPIO/m-p/585112#M21174</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by JohnR on Tue Oct 23 05:45:21 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I dno't think you can easily use the SSP. The convert pulse for the Linear converters is non-standard - they require a short pulse that starts the conversion rather than the normal chip select.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;NXP's AN11210 contains a description and example of the use of the SGPIO. I modified it to interface to a LTC1407A which reads out two sets of 14-bit data sequentially. I had to supply the conversion pulse from a separate GPIO output. I am still working on a version to read a single 14-bit conversion (LTC2355).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The SGPIO block is extremely flexible but complicated, at least to me, and the one NXP publication does not really give enough details of its usage. Also I found it difficult to relate some of the circuit blocks in the diagrams given in the UM10503 manual to the various configuration registers.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;John.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:11:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Help-me-choose-SSP-or-SGPIO/m-p/585112#M21174</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:11:02Z</dc:date>
    </item>
    <item>
      <title>Re: Help me choose: SSP or SGPIO</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Help-me-choose-SSP-or-SGPIO/m-p/585113#M21175</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by mark03 on Tue Oct 23 10:14:07 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Looking at the LT datasheet, I believe the conversion-start input can be a square wave (50% duty cycle).&amp;nbsp; Either way, it should be easy to make with a plain-old timer0/1/2/3 match output, assuming your application needs periodic sampling.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Another wrinkle is that to do this right, you should only have 16 SCLK cycles; active SCLK outside this time wastes power.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Is the SGPIO capable of being triggered somehow, in a one-shot fashion, by the falling edge of an input pin?&amp;nbsp; I need it to wait for the falling edge of BUSY, then zap out the 16 SCLKs while reading in the bits, then wait again for the next BUSY de-assertion.&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:11:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Help-me-choose-SSP-or-SGPIO/m-p/585113#M21175</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:11:03Z</dc:date>
    </item>
  </channel>
</rss>