<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i2c0 fails on port 1 lpc4088 in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/i2c0-fails-on-port-1-lpc4088/m-p/584602#M21072</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kenneth,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; When you run the I2C0 code on LPC4088, do you connect it with the according I2C slave device?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Please check the I2C communication wave, when the master send data, does slave give ACK feed back?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jingjing&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 06 Sep 2016 05:24:36 GMT</pubDate>
    <dc:creator>kerryzhou</dc:creator>
    <dc:date>2016-09-06T05:24:36Z</dc:date>
    <item>
      <title>i2c0 fails on port 1 lpc4088</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/i2c0-fails-on-port-1-lpc4088/m-p/584601#M21071</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When the lpc4088 or lpc4078 is configured to use port 1 pin 30 and 31 for i2c0 the device enters a busy state after the function&amp;nbsp; tmp = Chip_I2C_MasterSend(I2C0, hdmi_xfer.slaveAddr, hdmi_xfer.txBuff, hdmi_xfer.txSz); is executed.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Sep 2016 01:08:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/i2c0-fails-on-port-1-lpc4088/m-p/584601#M21071</guid>
      <dc:creator>kennethedlow</dc:creator>
      <dc:date>2016-09-02T01:08:01Z</dc:date>
    </item>
    <item>
      <title>Re: i2c0 fails on port 1 lpc4088</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/i2c0-fails-on-port-1-lpc4088/m-p/584602#M21072</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kenneth,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; When you run the I2C0 code on LPC4088, do you connect it with the according I2C slave device?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Please check the I2C communication wave, when the master send data, does slave give ACK feed back?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jingjing&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Sep 2016 05:24:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/i2c0-fails-on-port-1-lpc4088/m-p/584602#M21072</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2016-09-06T05:24:36Z</dc:date>
    </item>
  </channel>
</rss>