<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Finger print identification with LPC4357</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Finger-print-identification-with-LPC4357/m-p/584259#M21004</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by askar on Tue May 06 21:25:49 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi bavarian,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for your reply, the system that we use LPC4357 on it is a complete Time attendance system and we need to use&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;all devices of LPC4357 in it for example we need Ethernet, Usb host and device, MicroSD, Audio ,TFT LCD, Camera &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;and so on. currently we use Finger print modules purchased with high prices and the main price depends on Module's DSP pcb.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;we want to cancel DSP pcb and use only Finger Print sensor with our system.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Askar&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:07:57 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:07:57Z</dc:date>
    <item>
      <title>Finger print identification with LPC4357</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Finger-print-identification-with-LPC4357/m-p/584257#M21002</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by askar on Sat May 03 20:54:17 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Finger print modules usually have a DSP board often from TI or Analog devices that connect to a&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Finger print sensor and process finger print images come from sensor.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;when non DSP processors in market were operating in slow speeds, there was no way to replace&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;DSP processors with non DSP ones. i think that for medium size number of fingers, for example&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;templates of 100 to 200, we can use lpc4357 for identifying Finger print templates. is there any document&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;or effort on using lpc4357 for this field?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Best regards,&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:07:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Finger-print-identification-with-LPC4357/m-p/584257#M21002</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:07:55Z</dc:date>
    </item>
    <item>
      <title>Re: Finger print identification with LPC4357</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Finger-print-identification-with-LPC4357/m-p/584258#M21003</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by bavarian on Tue May 06 07:29:38 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Well, to be honest, the LPC4357 is a little bit oversized for that. Finger print modules are price sensitive components.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I would go for a version with reduced number of peripherals and maybe for the flashless version. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Then the code and constants can be in qSPI memory and some more time critical code would run from SRAM.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If you don't need floating point or 204MHz you could also use the LPC1800.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Bavarian&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:07:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Finger-print-identification-with-LPC4357/m-p/584258#M21003</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:07:56Z</dc:date>
    </item>
    <item>
      <title>Re: Finger print identification with LPC4357</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Finger-print-identification-with-LPC4357/m-p/584259#M21004</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by askar on Tue May 06 21:25:49 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi bavarian,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for your reply, the system that we use LPC4357 on it is a complete Time attendance system and we need to use&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;all devices of LPC4357 in it for example we need Ethernet, Usb host and device, MicroSD, Audio ,TFT LCD, Camera &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;and so on. currently we use Finger print modules purchased with high prices and the main price depends on Module's DSP pcb.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;we want to cancel DSP pcb and use only Finger Print sensor with our system.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Askar&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:07:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Finger-print-identification-with-LPC4357/m-p/584259#M21004</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:07:57Z</dc:date>
    </item>
  </channel>
</rss>