<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Incorrect LCDFP and LCDLP states with LCDEN disabled. in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Incorrect-LCDFP-and-LCDLP-states-with-LCDEN-disabled/m-p/583710#M20913</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by GregDavies on Wed Sep 16 08:35:44 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;In the user manual for the LCD Control register (Rev 1.6, p791), it states that when LCDEN is set to 0, then LCDLP, and LCDFP are set low. When I probe these lines, they are high in the disabled state. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have these pins both considered with:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- pulldown enabled&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- pullup disabled&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- input buffer enabled&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- glitch filter disabled&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- FP/LP functions selected. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;There's nothing in the errata about these pins resetting to an incorrect state. Is there more information I'm missing, or is this an error in the documentation or chip?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:08:26 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:08:26Z</dc:date>
    <item>
      <title>Incorrect LCDFP and LCDLP states with LCDEN disabled.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Incorrect-LCDFP-and-LCDLP-states-with-LCDEN-disabled/m-p/583710#M20913</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by GregDavies on Wed Sep 16 08:35:44 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;In the user manual for the LCD Control register (Rev 1.6, p791), it states that when LCDEN is set to 0, then LCDLP, and LCDFP are set low. When I probe these lines, they are high in the disabled state. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have these pins both considered with:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- pulldown enabled&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- pullup disabled&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- input buffer enabled&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- glitch filter disabled&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;- FP/LP functions selected. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;There's nothing in the errata about these pins resetting to an incorrect state. Is there more information I'm missing, or is this an error in the documentation or chip?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:08:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Incorrect-LCDFP-and-LCDLP-states-with-LCDEN-disabled/m-p/583710#M20913</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:08:26Z</dc:date>
    </item>
  </channel>
</rss>