<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPCOpen 2.16v + LPC4337 + ADC + DMA triggered by peripheral in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCOpen-2-16v-LPC4337-ADC-DMA-triggered-by-peripheral/m-p/583383#M20838</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by rob.konieczny on Sat Apr 16 00:07:37 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for suggestion but unfortunately it's not the case. I've configured DMA to use buffer which is 128 element long, not like in default LPCWare examples.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;DMA runs through whole buffer after being triggered only once by ADC.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 20:24:24 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T20:24:24Z</dc:date>
    <item>
      <title>LPCOpen 2.16v + LPC4337 + ADC + DMA triggered by peripheral</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCOpen-2-16v-LPC4337-ADC-DMA-triggered-by-peripheral/m-p/583381#M20836</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by rob.konieczny on Fri Apr 01 16:13:06 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Can someone give some example how to configure ADC and DMA in the way that DMA transfer is triggered by peripheral (GPDMA_TRANSFERTYPE_P2M_CONTROLLER_PERIPHERAL)?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I've tried on many ways but all the time with the same result - DMA triggered once, operates without waiting for next trigger from ADC. Like it would be GPDMA_TRANSFERTYPE_P2M_CONTROLLER_DMA.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Similar problem described here &lt;/SPAN&gt;&lt;A href="http://https://www.lpcware.com/content/forum/dma-adc-syncronizasion"&gt;DMA ADC sync&lt;/A&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks and regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Robert&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:24:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCOpen-2-16v-LPC4337-ADC-DMA-triggered-by-peripheral/m-p/583381#M20836</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:24:23Z</dc:date>
    </item>
    <item>
      <title>Re: LPCOpen 2.16v + LPC4337 + ADC + DMA triggered by peripheral</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCOpen-2-16v-LPC4337-ADC-DMA-triggered-by-peripheral/m-p/583382#M20837</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by thedaz on Sat Apr 09 02:59:31 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The reason is that one DMA transaction is executed only once then disables the DMA. The example defines a transfer size of one word. In order to have the DMA transfer another ADC sample you'll need to setup another transaction after the first completed. &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:24:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCOpen-2-16v-LPC4337-ADC-DMA-triggered-by-peripheral/m-p/583382#M20837</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:24:24Z</dc:date>
    </item>
    <item>
      <title>Re: LPCOpen 2.16v + LPC4337 + ADC + DMA triggered by peripheral</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCOpen-2-16v-LPC4337-ADC-DMA-triggered-by-peripheral/m-p/583383#M20838</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by rob.konieczny on Sat Apr 16 00:07:37 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks for suggestion but unfortunately it's not the case. I've configured DMA to use buffer which is 128 element long, not like in default LPCWare examples.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;DMA runs through whole buffer after being triggered only once by ADC.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:24:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCOpen-2-16v-LPC4337-ADC-DMA-triggered-by-peripheral/m-p/583383#M20838</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:24:24Z</dc:date>
    </item>
    <item>
      <title>Re: LPCOpen 2.16v + LPC4337 + ADC + DMA triggered by peripheral</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCOpen-2-16v-LPC4337-ADC-DMA-triggered-by-peripheral/m-p/583384#M20839</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;bump&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 19 Jun 2016 01:06:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCOpen-2-16v-LPC4337-ADC-DMA-triggered-by-peripheral/m-p/583384#M20839</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-19T01:06:59Z</dc:date>
    </item>
  </channel>
</rss>