<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SCT input detecting rising edge in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/SCT-input-detecting-rising-edge/m-p/582995#M20795</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by temp88 on Thu Mar 24 06:20:54 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;i'm using LPC43xx, and i need to count the number of rising edge of an external signal.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;i'd like to use SCT register for counting those edge (the signal is fast).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;i have some problem on setting up the chosen sct pin as input, or in finding some example code with sct timer used as input.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:08:25 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:08:25Z</dc:date>
    <item>
      <title>SCT input detecting rising edge</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SCT-input-detecting-rising-edge/m-p/582995#M20795</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by temp88 on Thu Mar 24 06:20:54 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;i'm using LPC43xx, and i need to count the number of rising edge of an external signal.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;i'd like to use SCT register for counting those edge (the signal is fast).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;i have some problem on setting up the chosen sct pin as input, or in finding some example code with sct timer used as input.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:08:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SCT-input-detecting-rising-edge/m-p/582995#M20795</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:08:25Z</dc:date>
    </item>
    <item>
      <title>Re: SCT input detecting rising edge</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SCT-input-detecting-rising-edge/m-p/582996#M20796</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;bump&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 19 Jun 2016 01:06:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SCT-input-detecting-rising-edge/m-p/582996#M20796</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-19T01:06:10Z</dc:date>
    </item>
  </channel>
</rss>