<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPCOpen V3.00 Feedback</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCOpen-V3-00-Feedback/m-p/582975#M20793</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by EarlBryner on Fri Dec 19 15:47:00 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Many new users struggle with the requirement to build the library projects in order to link the examples.&amp;nbsp; Could the projects be changed to refer to the library files directly?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Reply (Earl Bryner)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;This is understandable however the problem with making every project reference the lib files (like chip and board) directly is a maintenance issue.&amp;nbsp; If / when we need to add a new module to a library, we would then have to modify 30+ projects to include the new link which becomes a lot of extra work and introduces the possibility of missing one etc.&amp;nbsp; To help mitigate this problem, the LPCXpresso projects automatically have a dependency built in which forces the library to be built prior to linking.&amp;nbsp; I am not aware of a mechanism to enforce this in Keil or IAR.&amp;nbsp; There may be other creative ways to solve this problem so we are open to other suggestions.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 20:24:42 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T20:24:42Z</dc:date>
    <item>
      <title>LPCOpen V3.00 Feedback</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCOpen-V3-00-Feedback/m-p/582972#M20790</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by EarlBryner on Fri Dec 19 11:23:00 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Feedback on new V3.00 structure.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Please use the following guidelines to avoid topic fragmentation:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[list]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]If an existing subtopic exists, please use the 'Edit' button rather than 'Reply'.&amp;nbsp; Reply will start a new box which does not get attached to the original sub-topic. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; [*]When replying to subtopics it would be helpful to include your name to provide context on your perspective.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/list]&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:24:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCOpen-V3-00-Feedback/m-p/582972#M20790</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:24:40Z</dc:date>
    </item>
    <item>
      <title>Re: LPCOpen V3.00 Feedback</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCOpen-V3-00-Feedback/m-p/582973#M20791</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by EarlBryner on Fri Dec 19 11:59:00 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The new paths are indeed shorter, but can we shorten them further (i.e change the project dir lpcxpresso to lpx)?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Reply (Earl Bryner):&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;This is a touchy subject. The current paths were developed as a compromise between competing desires to shorten the folder names and lengthening them to be more descriptive. The current proposal is the resulting compromise between those interest.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:24:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCOpen-V3-00-Feedback/m-p/582973#M20791</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:24:40Z</dc:date>
    </item>
    <item>
      <title>Re: LPCOpen V3.00 Feedback</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCOpen-V3-00-Feedback/m-p/582974#M20792</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by EarlBryner on Fri Dec 19 12:44:00 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Can the example and project files be grouped together to aid in distribution?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Reply (Earl Bryner):&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The current proposal (though this wasn't obvious in the sample provided) has separate folders for projects and source because the intention is that when a MCU family has multiple boards (virtually every MCU we have fits into this case), there will be a unique project directory for each board.&amp;nbsp; For example in the provided sample if we were to include support for the original CSP board we would have included a prj_lpcxpresso_54102_csp directory which would have had iar, keil and lpcxpresso sub directories similar to the current prj_lpcxpresso_54102 directory.&amp;nbsp;&amp;nbsp; Additionally in order to support vertical markets it is very desirable to have a clear distinction between source code and project files since they are typically only interested in the source code (because they maintain their own project files).&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:24:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCOpen-V3-00-Feedback/m-p/582974#M20792</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:24:41Z</dc:date>
    </item>
    <item>
      <title>Re: LPCOpen V3.00 Feedback</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCOpen-V3-00-Feedback/m-p/582975#M20793</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by EarlBryner on Fri Dec 19 15:47:00 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Many new users struggle with the requirement to build the library projects in order to link the examples.&amp;nbsp; Could the projects be changed to refer to the library files directly?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Reply (Earl Bryner)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;This is understandable however the problem with making every project reference the lib files (like chip and board) directly is a maintenance issue.&amp;nbsp; If / when we need to add a new module to a library, we would then have to modify 30+ projects to include the new link which becomes a lot of extra work and introduces the possibility of missing one etc.&amp;nbsp; To help mitigate this problem, the LPCXpresso projects automatically have a dependency built in which forces the library to be built prior to linking.&amp;nbsp; I am not aware of a mechanism to enforce this in Keil or IAR.&amp;nbsp; There may be other creative ways to solve this problem so we are open to other suggestions.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:24:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCOpen-V3-00-Feedback/m-p/582975#M20793</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:24:42Z</dc:date>
    </item>
    <item>
      <title>Re: LPCOpen V3.00 Feedback</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCOpen-V3-00-Feedback/m-p/582976#M20794</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by EarlBryner on Fri Dec 19 15:57:09 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Most examples share common code (such as startup files) which makes it difficult to customize for only a specific example.&amp;nbsp; Can the examples be changed to have their own copy instead of sharing?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Reply (Earl Bryner)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Our experience (please correct me if I am wrong) has been that the desire to customize startup code is the exception rather than the rule.&amp;nbsp; Sharing the startup code across examples allows us to easily correct bugs / add features across all the examples rather than having to replicate the fix N times for each example.&amp;nbsp; In the rare case that an example needs a custom startup file, it should be relatively easy to copy the shared one to the local project source directory and reference it from the project.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:24:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCOpen-V3-00-Feedback/m-p/582976#M20794</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:24:42Z</dc:date>
    </item>
  </channel>
</rss>