<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: lpc4350 PDL USB CDC Example</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpc4350-PDL-USB-CDC-Example/m-p/582634#M20711</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by nxpUSBlib team on Tue Aug 07 14:52:32 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The problem with the CDC locking up has been resolved and will be in the next release of nxpUSBlib due out in October.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In the meantime, you can tell nxpUSBlib to use the built-in ROM drivers by setting USE_USB_ROM_STACK to 1 in nxpUSBlibConfig.h&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:06:52 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:06:52Z</dc:date>
    <item>
      <title>lpc4350 PDL USB CDC Example</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpc4350-PDL-USB-CDC-Example/m-p/582632#M20709</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by gregd on Wed Jan 18 09:24:14 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I am working on getting the USB CDC example running that is included in the LPC43xx PDL.&amp;nbsp; The application on the Hitex LPC43xx board seems to run fine, but I am having problems getting the pc USB driver installed to work with this example. Do you have any additional information on how to get this driver installed on the pc?&amp;nbsp; I am running Windows 7.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Additionally, in the Abstract.txt files that are included with each example, they refer to the “LPC43xx Example Description” document.&amp;nbsp; Do you know where I can get a copy of this?&amp;nbsp; It doesn’t seem to be included in the LPC43xx PDL zip file.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any additional resources you may be able to find related to using the USB on the LPC43xx for CDC would be appreciated.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Greg Dunn&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;304-542-4383&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A class="jive-link-email-small" href="mailto:greg.dunn@eagleresearchcorp.com"&gt;greg.dunn@eagleresearchcorp.com&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:06:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lpc4350-PDL-USB-CDC-Example/m-p/582632#M20709</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:06:50Z</dc:date>
    </item>
    <item>
      <title>Re: lpc4350 PDL USB CDC Example</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpc4350-PDL-USB-CDC-Example/m-p/582633#M20710</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by gregd on Thu Jan 19 07:28:10 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;After playing around with the inf file and looking at the inf file included with the nxpUSBLib, I was able to create a version that successfully installed the driver on Windows 7 64 bit.&amp;nbsp; The USB CDC example works OK for a while but then appears to lock up for some reason.&amp;nbsp; If you send several strings of characters the USB port will lock up and you have to restart the program on the LPC4350 to recover.&amp;nbsp; Any ideas on how to fix this problem?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I also noticed that the CDC example does not use the internal ROM drivers.&amp;nbsp; Is there any plans to release an example that shows how to use the internal ROM CDC driver?&amp;nbsp; I assume that the internal ROM CDC driver does work.&amp;nbsp; Is this a correct assumption?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Greg Dunn&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;304-542-4383&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A class="jive-link-email-small" href="mailto:greg.dunn@eagleresearchcorp.com"&gt;greg.dunn@eagleresearchcorp.com&lt;/A&gt;&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:06:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lpc4350-PDL-USB-CDC-Example/m-p/582633#M20710</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:06:51Z</dc:date>
    </item>
    <item>
      <title>Re: lpc4350 PDL USB CDC Example</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpc4350-PDL-USB-CDC-Example/m-p/582634#M20711</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by nxpUSBlib team on Tue Aug 07 14:52:32 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;The problem with the CDC locking up has been resolved and will be in the next release of nxpUSBlib due out in October.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In the meantime, you can tell nxpUSBlib to use the built-in ROM drivers by setting USE_USB_ROM_STACK to 1 in nxpUSBlibConfig.h&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:06:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lpc4350-PDL-USB-CDC-Example/m-p/582634#M20711</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:06:52Z</dc:date>
    </item>
  </channel>
</rss>