<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 LPC USB CDC Example Project Code Bugs</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-USB-CDC-Example-Project-Code-Bugs/m-p/582480#M20688</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by rlund on Thu Oct 16 12:40:42 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I found two bug/issue/artifacts referenced in the USB CDC example project: usbd_rom_cdc_vcom.&amp;nbsp; One is "artf42016" and one is "artf45032".&amp;nbsp; The code related to these artifacts can by found in the project by searching the artifact numbers.&amp;nbsp; The workaround for these USB ROM "artifacts" is contained within the example project code, as opposed to fixing it at the source, in the library itself.&amp;nbsp; I have two questions:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Where/how can I find out more information about these two artifacts?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Are there other artifacts or bugs out there that I should be wary of with this code?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any information or help on where to start answering these questions would be greatly appreciated.&amp;nbsp; Thanks!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 20:23:24 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T20:23:24Z</dc:date>
    <item>
      <title>LPC USB CDC Example Project Code Bugs</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-USB-CDC-Example-Project-Code-Bugs/m-p/582480#M20688</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by rlund on Thu Oct 16 12:40:42 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I found two bug/issue/artifacts referenced in the USB CDC example project: usbd_rom_cdc_vcom.&amp;nbsp; One is "artf42016" and one is "artf45032".&amp;nbsp; The code related to these artifacts can by found in the project by searching the artifact numbers.&amp;nbsp; The workaround for these USB ROM "artifacts" is contained within the example project code, as opposed to fixing it at the source, in the library itself.&amp;nbsp; I have two questions:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Where/how can I find out more information about these two artifacts?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Are there other artifacts or bugs out there that I should be wary of with this code?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any information or help on where to start answering these questions would be greatly appreciated.&amp;nbsp; Thanks!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:23:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-USB-CDC-Example-Project-Code-Bugs/m-p/582480#M20688</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:23:24Z</dc:date>
    </item>
  </channel>
</rss>