<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Can the script in LPCScrypt able to program more than 1 simultaneously</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-the-script-in-LPCScrypt-able-to-program-more-than-1/m-p/582160#M20606</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by r43125 on Tue May 24 01:57:02 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;With reference to Chapter 6 Appendix, It mentioned that multiple serial port, does it meant that we could write script in the LPCscrypt to be able to program more than 1 boards simultaneously or one at the time. Customer would like to program more than one more at one time, can it work for LPC4350.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Audrey&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;6.1 Multiple serial ports&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When LPCScrypt firware is booted, it will enumerate on the host as a USB serial (VCOM)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;port. In normal operation LPCScrypt (host) will be able to detect and use the correct&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;serial port automatically. However this automatic detection cannot identify the port to use&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;if multiple USB serial ports are found. The solution is to manually identify the correct serial&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;port and specify it to LPCScrypt using the -d switch.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:05:28 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:05:28Z</dc:date>
    <item>
      <title>Can the script in LPCScrypt able to program more than 1 simultaneously</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-the-script-in-LPCScrypt-able-to-program-more-than-1/m-p/582160#M20606</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by r43125 on Tue May 24 01:57:02 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;With reference to Chapter 6 Appendix, It mentioned that multiple serial port, does it meant that we could write script in the LPCscrypt to be able to program more than 1 boards simultaneously or one at the time. Customer would like to program more than one more at one time, can it work for LPC4350.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Audrey&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;6.1 Multiple serial ports&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When LPCScrypt firware is booted, it will enumerate on the host as a USB serial (VCOM)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;port. In normal operation LPCScrypt (host) will be able to detect and use the correct&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;serial port automatically. However this automatic detection cannot identify the port to use&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;if multiple USB serial ports are found. The solution is to manually identify the correct serial&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;port and specify it to LPCScrypt using the -d switch.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:05:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-the-script-in-LPCScrypt-able-to-program-more-than-1/m-p/582160#M20606</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:05:28Z</dc:date>
    </item>
    <item>
      <title>Re: Can the script in LPCScrypt able to program more than 1 simultaneously</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-the-script-in-LPCScrypt-able-to-program-more-than-1/m-p/582161#M20607</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by lpcxpresso-support on Tue May 24 08:13:13 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;From a single host 'PC' you could have more than one board connected and program them via LPCScrypt. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;As described you can refer to the individual connection using the -d &amp;lt;comport&amp;gt; switch.&amp;nbsp; e.g.:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;bin\lpcscrypt -d comport1 command
bin\lpcscrypt -d comport2 command&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Some notes:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;[list]&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]A single invocation of LPCScrypt on the host can only communicate with a single board at a time.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;nbsp; [*]The LPCScrypt boot process will only operate if a single LPC device (with vid/pid of 0x1FC9/0x000C) is visible over USB i.e. you cannot connect two LPC devices and boot them both sequentially. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[/list]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Yours,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;LPCXpresso-support&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:05:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-the-script-in-LPCScrypt-able-to-program-more-than-1/m-p/582161#M20607</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:05:29Z</dc:date>
    </item>
    <item>
      <title>Re: Can the script in LPCScrypt able to program more than 1 simultaneously</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-the-script-in-LPCScrypt-able-to-program-more-than-1/m-p/582162#M20608</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;bump&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 19 Jun 2016 01:11:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-the-script-in-LPCScrypt-able-to-program-more-than-1/m-p/582162#M20608</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-19T01:11:38Z</dc:date>
    </item>
  </channel>
</rss>