<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックI²C with CDL library - CMSIS compatibility problem</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/I-C-with-CDL-library-CMSIS-compatibility-problem/m-p/581958#M20562</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by L.simon on Fri Apr 11 07:28:37 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;hello everyone,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;i need to get USB and I²C going on a LPC4357 and got the usb part working with the nxpUSBlib.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;This library works with CDL and untill now didn't ive any problems, i also have a program for I2C working with the CMSIS library&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;i thought the cmsis library was compatible to the CDL library so i tried to run the I2C program on the CDL lib.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;this compiles just fine but while running gets stuck in the while loop in the function I2C_Start()&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;it seems the I2C interrupt flag doesn't work right, the status (STAT) is 0xF8 which means 'no relevant state info available'&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;i have no id what to do next!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;any help is appreciated!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks in advance,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Simon&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:06:22 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:06:22Z</dc:date>
    <item>
      <title>I²C with CDL library - CMSIS compatibility problem</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/I-C-with-CDL-library-CMSIS-compatibility-problem/m-p/581958#M20562</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by L.simon on Fri Apr 11 07:28:37 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;hello everyone,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;i need to get USB and I²C going on a LPC4357 and got the usb part working with the nxpUSBlib.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;This library works with CDL and untill now didn't ive any problems, i also have a program for I2C working with the CMSIS library&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;i thought the cmsis library was compatible to the CDL library so i tried to run the I2C program on the CDL lib.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;this compiles just fine but while running gets stuck in the while loop in the function I2C_Start()&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;it seems the I2C interrupt flag doesn't work right, the status (STAT) is 0xF8 which means 'no relevant state info available'&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;i have no id what to do next!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;any help is appreciated!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks in advance,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Simon&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:06:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/I-C-with-CDL-library-CMSIS-compatibility-problem/m-p/581958#M20562</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:06:22Z</dc:date>
    </item>
    <item>
      <title>Re: I²C with CDL library - CMSIS compatibility problem</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/I-C-with-CDL-library-CMSIS-compatibility-problem/m-p/581959#M20563</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by L.simon on Thu Apr 17 05:35:14 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;sorry, i changed the clock settings in the CMSIS library and forgot to do the same in the CDL library&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;it works fine now&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:06:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/I-C-with-CDL-library-CMSIS-compatibility-problem/m-p/581959#M20563</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:06:23Z</dc:date>
    </item>
  </channel>
</rss>