<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Isp mode from user code</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Isp-mode-from-user-code/m-p/581297#M20408</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your message,&lt;BR /&gt;But for sure ISP is supported by CAN in the LPC11C24, I did software download many times with Flash magic tool (free).&lt;/P&gt;&lt;P&gt;Unfortunately, the only way I know to set the lpc in ISP mode is by a hardware reset while I need to do it by CAN (by user code).&lt;BR /&gt;Best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 01 Sep 2016 05:55:18 GMT</pubDate>
    <dc:creator>gfa</dc:creator>
    <dc:date>2016-09-01T05:55:18Z</dc:date>
    <item>
      <title>Isp mode from user code</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Isp-mode-from-user-code/m-p/581295#M20406</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using a LPC11C24 (with integrated CAN bus transceiver) and I need to write a function to go to CAN ISP mode from my user code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this possible and how ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Aug 2016 13:24:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Isp-mode-from-user-code/m-p/581295#M20406</guid>
      <dc:creator>gfa</dc:creator>
      <dc:date>2016-08-31T13:24:13Z</dc:date>
    </item>
    <item>
      <title>Re: Isp mode from user code</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Isp-mode-from-user-code/m-p/581296#M20407</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="286920" data-username="gfa" href="https://community.nxp.com/people/gfa"&gt;Guillaume FANJAS&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;The integrated ISP doesn't support the CAN interface.&lt;/P&gt;&lt;P&gt;In my opinion, you need to create a CAN bootloader for the implementation and you can refer to the attachment about the bootlaoder design.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Sep 2016 02:40:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Isp-mode-from-user-code/m-p/581296#M20407</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-09-01T02:40:00Z</dc:date>
    </item>
    <item>
      <title>Re: Isp mode from user code</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Isp-mode-from-user-code/m-p/581297#M20408</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your message,&lt;BR /&gt;But for sure ISP is supported by CAN in the LPC11C24, I did software download many times with Flash magic tool (free).&lt;/P&gt;&lt;P&gt;Unfortunately, the only way I know to set the lpc in ISP mode is by a hardware reset while I need to do it by CAN (by user code).&lt;BR /&gt;Best regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Sep 2016 05:55:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Isp-mode-from-user-code/m-p/581297#M20408</guid>
      <dc:creator>gfa</dc:creator>
      <dc:date>2016-09-01T05:55:18Z</dc:date>
    </item>
    <item>
      <title>Re: Isp mode from user code</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Isp-mode-from-user-code/m-p/581298#M20409</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-containerid="-1" data-containertype="-1" data-content-finding="Community" data-objectid="286920" data-objecttype="3" href="https://community.nxp.com/people/gfa"&gt;Guillaume FANJAS&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Yes, the LPC11C24 supports the UART ISP and CAN ISP routines.&lt;/P&gt;&lt;P&gt;Sorry, I miss the information.&lt;/P&gt;&lt;P&gt;You can use the IAR command to force the LPC11C24 enter into the ISP mode.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="2016-09-01_15-21-31.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/3872i5CAF99C586E55872/image-size/large?v=v2&amp;amp;px=999" role="button" title="2016-09-01_15-21-31.jpg" alt="2016-09-01_15-21-31.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Sep 2016 07:25:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Isp-mode-from-user-code/m-p/581298#M20409</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2016-09-01T07:25:53Z</dc:date>
    </item>
  </channel>
</rss>