<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックMCPWM driver</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/MCPWM-driver/m-p/581057#M20346</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by swiebertje on Tue Nov 25 07:03:19 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi there,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;We're migrating our custom LPC4357 board support package from CMSIS to LPCOPEN. In CMSIS there was a Motor Control PWM driver which is missing from LPCOPEN (2.12). I noticed that the SCT is now used for generating a PWM. Our board is wired to use P4_0 as a PWM output pin but this pin is not configurable to be used as a SCT output.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;For now I think the only way to overcome this is to keep using the CMSIS MCPWM driver?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I was wondering if MCPWM will be supported by LPCOPEN in the future?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 20:20:32 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T20:20:32Z</dc:date>
    <item>
      <title>MCPWM driver</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/MCPWM-driver/m-p/581057#M20346</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by swiebertje on Tue Nov 25 07:03:19 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi there,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;We're migrating our custom LPC4357 board support package from CMSIS to LPCOPEN. In CMSIS there was a Motor Control PWM driver which is missing from LPCOPEN (2.12). I noticed that the SCT is now used for generating a PWM. Our board is wired to use P4_0 as a PWM output pin but this pin is not configurable to be used as a SCT output.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;For now I think the only way to overcome this is to keep using the CMSIS MCPWM driver?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I was wondering if MCPWM will be supported by LPCOPEN in the future?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 20:20:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/MCPWM-driver/m-p/581057#M20346</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T20:20:32Z</dc:date>
    </item>
  </channel>
</rss>