<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックWeird clock issue</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Weird-clock-issue/m-p/581036#M20340</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Algorithm on Thu Aug 13 14:42:12 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hullo guys, I'm using KEIL as the IDE to program LPC4357 . I have a problem with the CGU, as it says in the user manual , the BASE_M4_CLK is provided by the PLL1 by default. But in the register description of the BASE_M4_CLK register, the user manual says it is connected to the IRC by default !!! . When I started debugging in KEIL, without any system initialization (removed it from the assembly start-up code) , I found that KEIL is missing IDIVC and IDIVD registers !!! and also the BASE_M4_CLK register in the debugger is connected to the IDIVC !! &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The attached picture shows it all. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I also noticed that the LPC library is missing the CCU .h and .c files. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Any explanation ??!!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:06:47 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:06:47Z</dc:date>
    <item>
      <title>Weird clock issue</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Weird-clock-issue/m-p/581036#M20340</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Algorithm on Thu Aug 13 14:42:12 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hullo guys, I'm using KEIL as the IDE to program LPC4357 . I have a problem with the CGU, as it says in the user manual , the BASE_M4_CLK is provided by the PLL1 by default. But in the register description of the BASE_M4_CLK register, the user manual says it is connected to the IRC by default !!! . When I started debugging in KEIL, without any system initialization (removed it from the assembly start-up code) , I found that KEIL is missing IDIVC and IDIVD registers !!! and also the BASE_M4_CLK register in the debugger is connected to the IDIVC !! &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The attached picture shows it all. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I also noticed that the LPC library is missing the CCU .h and .c files. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Any explanation ??!!&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:06:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Weird-clock-issue/m-p/581036#M20340</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:06:47Z</dc:date>
    </item>
  </channel>
</rss>