<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC4357-EVB write and read file to SD eMMC in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357-EVB-write-and-read-file-to-SD-eMMC/m-p/580176#M20180</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by nxpecosystem on Fri May 06 14:07:12 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;There is a full size SD card on the Hitex LPC4350 eval board, and on the LPC General Purpose Shield (which can be used with an LPCXpresso4337/4367 board.) LPCOpen packages for these boards include examples for read/write to a memory card over the SD eMMC interface. Hopefully these can help you out.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:05:41 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:05:41Z</dc:date>
    <item>
      <title>LPC4357-EVB write and read file to SD eMMC</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357-EVB-write-and-read-file-to-SD-eMMC/m-p/580175#M20179</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by marcosbontempo on Fri May 06 06:43:10 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Hello,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using a LPC4357-EVB kit, which has a SD eMMC interface. I found this example that reads a WAV file from the SD and plays it:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fwww.element14.com%2Fcommunity%2Fdocs%2FDOC-62637" rel="nofollow" target="_blank"&gt;https://www.element14.com/community/docs/DOC-62637&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;However, I also need to write a file into the SD. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Does anybody have a simple example that manipulates files in a SD card, using the LPC4357?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Any tip wil be very helpful,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:05:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357-EVB-write-and-read-file-to-SD-eMMC/m-p/580175#M20179</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:05:40Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4357-EVB write and read file to SD eMMC</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357-EVB-write-and-read-file-to-SD-eMMC/m-p/580176#M20180</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by nxpecosystem on Fri May 06 14:07:12 MST 2016&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;There is a full size SD card on the Hitex LPC4350 eval board, and on the LPC General Purpose Shield (which can be used with an LPCXpresso4337/4367 board.) LPCOpen packages for these boards include examples for read/write to a memory card over the SD eMMC interface. Hopefully these can help you out.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:05:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357-EVB-write-and-read-file-to-SD-eMMC/m-p/580176#M20180</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:05:41Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4357-EVB write and read file to SD eMMC</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357-EVB-write-and-read-file-to-SD-eMMC/m-p/580177#M20181</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;bump&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 19 Jun 2016 01:10:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357-EVB-write-and-read-file-to-SD-eMMC/m-p/580177#M20181</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-19T01:10:07Z</dc:date>
    </item>
  </channel>
</rss>