<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックProblem using ADC on LPC1549</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-using-ADC-on-LPC1549/m-p/580159#M20177</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am modifying the periph_adc_rom example and everything works fine if i read a single channel like in the original example.&lt;/P&gt;&lt;P&gt;When I tried to modify the example to use two channels I can read the value from the channels but the values are&amp;nbsp;about 10% lower than what I expect.&lt;BR /&gt;Did anybody find the same issue?&lt;/P&gt;&lt;P&gt;Thank you very much in advance for your help&lt;/P&gt;&lt;P&gt;Please find attached my code.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338019"&gt;adc_rom.c.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 31 Aug 2016 16:04:21 GMT</pubDate>
    <dc:creator>stefanobertazzo</dc:creator>
    <dc:date>2016-08-31T16:04:21Z</dc:date>
    <item>
      <title>Problem using ADC on LPC1549</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-using-ADC-on-LPC1549/m-p/580159#M20177</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am modifying the periph_adc_rom example and everything works fine if i read a single channel like in the original example.&lt;/P&gt;&lt;P&gt;When I tried to modify the example to use two channels I can read the value from the channels but the values are&amp;nbsp;about 10% lower than what I expect.&lt;BR /&gt;Did anybody find the same issue?&lt;/P&gt;&lt;P&gt;Thank you very much in advance for your help&lt;/P&gt;&lt;P&gt;Please find attached my code.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338019"&gt;adc_rom.c.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Aug 2016 16:04:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-using-ADC-on-LPC1549/m-p/580159#M20177</guid>
      <dc:creator>stefanobertazzo</dc:creator>
      <dc:date>2016-08-31T16:04:21Z</dc:date>
    </item>
    <item>
      <title>Re: Problem using ADC on LPC1549</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-using-ADC-on-LPC1549/m-p/580160#M20178</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check the AN10974 &lt;A class="link-titled" href="http://www.nxp.com/documents/application_note/AN10974.pdf" title="http://www.nxp.com/documents/application_note/AN10974.pdf"&gt;http://www.nxp.com/documents/application_note/AN10974.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This application note,&amp;nbsp; provides general design guidelines that can be applied to the board layout design, as well as a reference design and a software project the user can utilize in order to test the LPC1700 12-bit ADC. Some test scenarios are also included, demonstrating the factors that can affect the conversion results.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Dec 2016 15:01:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-using-ADC-on-LPC1549/m-p/580160#M20178</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2016-12-13T15:01:17Z</dc:date>
    </item>
  </channel>
</rss>