<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックUsing LPCOpen with Keil uVision on Keil MCB 4350 board</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-LPCOpen-with-Keil-uVision-on-Keil-MCB-4350-board/m-p/579527#M20061</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jrodrig67 on Wed Feb 12 05:10:51 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Dear members,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am new to the NXP MCUs and to the Keil environment. Also to LPCOpen. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;So no wonder I am running into issues.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;My question is simple. I am familiarising myself with my development environment using the stuff in the subject of the post.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Ideally, I would like to use a package lpcopen_2_04_keil_iar_keil_mcb_4350, but since it does not exist, I had to settle for using lpcopen_2_04_keil_iar_keil_mcb_4357; i.e. I am using a different CPU/development board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have started with the freertos_blinky example. I changed my configuration to target the LCP4350 instead of the LCP4357; taking the examples provided with the Keil uVision environment (C:\Keil\ARM\Boards\Keil\MCB4300\Blinky) but I get very strange behavior like obvious breakpoints not hit, flash verification errors (not all the time), things like that.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So my questions are:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;1) Does someone have the equivalent of lpcopen_2_04_keil_iar_keil_mcb_4357 ported to the mcb_4350?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2) If that is not the case, what changes will I need to make in the Keil projects to use the 4350?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance for your time.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Juan Rodriguez&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:03:30 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:03:30Z</dc:date>
    <item>
      <title>Using LPCOpen with Keil uVision on Keil MCB 4350 board</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-LPCOpen-with-Keil-uVision-on-Keil-MCB-4350-board/m-p/579527#M20061</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by jrodrig67 on Wed Feb 12 05:10:51 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Dear members,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am new to the NXP MCUs and to the Keil environment. Also to LPCOpen. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;So no wonder I am running into issues.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;My question is simple. I am familiarising myself with my development environment using the stuff in the subject of the post.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Ideally, I would like to use a package lpcopen_2_04_keil_iar_keil_mcb_4350, but since it does not exist, I had to settle for using lpcopen_2_04_keil_iar_keil_mcb_4357; i.e. I am using a different CPU/development board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I have started with the freertos_blinky example. I changed my configuration to target the LCP4350 instead of the LCP4357; taking the examples provided with the Keil uVision environment (C:\Keil\ARM\Boards\Keil\MCB4300\Blinky) but I get very strange behavior like obvious breakpoints not hit, flash verification errors (not all the time), things like that.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;So my questions are:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;1) Does someone have the equivalent of lpcopen_2_04_keil_iar_keil_mcb_4357 ported to the mcb_4350?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;2) If that is not the case, what changes will I need to make in the Keil projects to use the 4350?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks in advance for your time.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Juan Rodriguez&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:03:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Using-LPCOpen-with-Keil-uVision-on-Keil-MCB-4350-board/m-p/579527#M20061</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:03:30Z</dc:date>
    </item>
    <item>
      <title>Re: Using LPCOpen with Keil uVision on Keil MCB 4350 board</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-LPCOpen-with-Keil-uVision-on-Keil-MCB-4350-board/m-p/579528#M20062</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by xianghuiwang on Thu Apr 17 17:26:10 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi, Juan,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;For debugging purpose, you can change the C/C++ optimization level of both libs and the application project from the default Level 3 (-O3) to Level 0 (-O0) from the Keil compiler under the "Options for Target".&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;After this, you should be able to hit all the break points you intended.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Since you can hit some break points, I think you conversion from flash to ram is working in general. General steps to convert from flash to ram target are:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;a. change target map.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;b. use Keil .ini file to setup SP and PC. The ram.ini file is included in the lpcopen package for your reference.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Good luck!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:03:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Using-LPCOpen-with-Keil-uVision-on-Keil-MCB-4350-board/m-p/579528#M20062</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:03:31Z</dc:date>
    </item>
  </channel>
</rss>