<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックUSB CDC Driver on MAC OSX</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-CDC-Driver-on-MAC-OSX/m-p/579385#M20025</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We developed a USB data acquisition equipment with LPC4370, the product works&amp;nbsp;well on Windows, and now we'd like to migrate it to MAC OSX. The first problem is the USB data exchange between LPC4370 and MAC OSX, do we need a specific driver for USB CDC on MAC OSX?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any example of USB application on MAC OSX using LPC? &amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 31 Aug 2016 13:31:13 GMT</pubDate>
    <dc:creator>damihuanghuang</dc:creator>
    <dc:date>2016-08-31T13:31:13Z</dc:date>
    <item>
      <title>USB CDC Driver on MAC OSX</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-CDC-Driver-on-MAC-OSX/m-p/579385#M20025</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We developed a USB data acquisition equipment with LPC4370, the product works&amp;nbsp;well on Windows, and now we'd like to migrate it to MAC OSX. The first problem is the USB data exchange between LPC4370 and MAC OSX, do we need a specific driver for USB CDC on MAC OSX?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any example of USB application on MAC OSX using LPC? &amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Aug 2016 13:31:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB-CDC-Driver-on-MAC-OSX/m-p/579385#M20025</guid>
      <dc:creator>damihuanghuang</dc:creator>
      <dc:date>2016-08-31T13:31:13Z</dc:date>
    </item>
    <item>
      <title>Re: USB CDC Driver on MAC OSX</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB-CDC-Driver-on-MAC-OSX/m-p/579386#M20026</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you have an LPC4370 based system which creates a USB CDC connection to the outside world, then if you connect this to the USB port on a Mac, then&amp;nbsp;Mac OS X should automatically detect the USB CDC connection using its built in drivers. The simplest way to see what is available&amp;nbsp;is to open a terminal and enter "ls /dev/tty.usb* which should give you a list of USB virtual serial ports. You can then use the built in "screen" terminal &amp;nbsp;(or something like CoolTerm) to talk to it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To access it via anything other than a terminal program, you will then need to use the standard OS APIs. Lots more info if you use your favourite internet search engine - for example :&amp;nbsp;&lt;A class="link-titled" href="https://www.mac-usb-serial.com/wordpress/serial-port-programming-swift-mac-os-x/" title="https://www.mac-usb-serial.com/wordpress/serial-port-programming-swift-mac-os-x/"&gt;Mac OS X Drivers for CH340 / CH341 / PL2303 USB to RS-232 Devices&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Sep 2016 10:53:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB-CDC-Driver-on-MAC-OSX/m-p/579386#M20026</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2016-09-01T10:53:01Z</dc:date>
    </item>
  </channel>
</rss>