<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: 4 x SDRAM at LPC43x7</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/4-x-SDRAM-at-LPC43x7/m-p/578989#M19926</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by khfreiberg on Tue Dec 03 10:53:15 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have this Excel sheet. I tested at lower clock speed and the behavior changed. I still have this jump in address. I am filling the RAM with up-counting values, and read it back immediately after filling. That works fine. But when I read it back later on using an USB interface or even a RAM window in uVision I see this jump of 4 bit back in address. Thanks for the mode set up. What's still confusing me is 'LPC_EMC-&amp;gt;DYNAMICREFRESH'. When I read the manual I should use '7.8us * 204MHz/2 / 16(+1) cycl'. But in examples I see two programmings where the second call deals with '15625'. I have no clue where this number is coming from. Additionally, I do not see how examples matches the initialization procedure in the RAM data sheet. It talks about two 'AUTO REFRESH' cycles. I assume this is the 'PALL' command. I see only one. But I see multiple NOP commands. What are they doing? This is the magic I mean ;-))&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Greetings,&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:02:12 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:02:12Z</dc:date>
    <item>
      <title>4 x SDRAM at LPC43x7</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/4-x-SDRAM-at-LPC43x7/m-p/578987#M19924</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by khfreiberg on Mon Dec 02 16:23:12 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have 4 x MT48LC64M8A2 (-75) at dynCS1 to use the full 256MB. It is a brand new prototype board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;EMC is running at 204/2MHz. I have problems with the setup. My little RAM test works fine at first run. But when I read the data again they change. The changed data seems to be stable with a '00' in chip 1 and 'FF' in chip 2. Other data are shifted by 4 byte in address. Looks like a refresh issue. I would like to distinguish between layout problem and setup failure. But when I search examples and forum entries it seems like everybody has it's own magic. Especially strange is the multiple calling of 'LPC_EMC-&amp;gt;DYNAMICREFRESH' where the shown values doesn't match 'UM10503'. Additionally I am not sure how to calculate the offset for WR_MODE (12?, 14?) for 4 chips. Both values don't change behavior. Does anybody have a working setup that I can use as platform for further investigations?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I would appreciate any help.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Greetings&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:02:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/4-x-SDRAM-at-LPC43x7/m-p/578987#M19924</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:02:11Z</dc:date>
    </item>
    <item>
      <title>Re: 4 x SDRAM at LPC43x7</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/4-x-SDRAM-at-LPC43x7/m-p/578988#M19925</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by bavarian on Tue Dec 03 09:42:02 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi, &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;my first recommendation is that you test your setup at a lower SDRAM speed. Maybe you've done everything correct but you run into the problem EMC.1 described in the error sheet.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;If it works at lower speed the workaround could be to add a small capacitor (5 ... 15pF) to the SDRAM_CLK to delay the clock signal a little bit.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The correct initialization of the SDRAM is of course important, but not really magic.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I attached an Excel file which might help with the register programming.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It is for the MT48LC4M32B2, you need to adapt it to the MT48LC64M8A2 &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The mode register:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;DIV class="j-rte-table"&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca" style="border:1px solid black;background-color:#cacaca;"&gt; &lt;PRE&gt;// Write the SDRAM mode register
// Mode register bits: see also data sheet of the SDRAM
// M0-M2 specify the burst length: 011 = burst length of 8 (always!!)
// M3 specifies the type of burst (sequential or interleaved): 0 = sequential (always!!)
// M4- M6 specify the CAS latency: 2 
// M7 and M8 specify the operating mode: 00 = standard operation (always!!)
// M9 specifies the WRITE burst mode: 0 = programmed burst length&amp;nbsp; (always!!)
// M10 and M11 are reserved for future use
//
// This mode register value needs to be shifted by a specific number of bits:
// Column address bits: 10&amp;nbsp; (A0 - A9)
// 4 banks:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 2
// RBC mapping:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1
//&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ---
//&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 13&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;/DIV&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Hope this brings you forward,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;NXP Support Team&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:02:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/4-x-SDRAM-at-LPC43x7/m-p/578988#M19925</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:02:12Z</dc:date>
    </item>
    <item>
      <title>Re: 4 x SDRAM at LPC43x7</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/4-x-SDRAM-at-LPC43x7/m-p/578989#M19926</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by khfreiberg on Tue Dec 03 10:53:15 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I have this Excel sheet. I tested at lower clock speed and the behavior changed. I still have this jump in address. I am filling the RAM with up-counting values, and read it back immediately after filling. That works fine. But when I read it back later on using an USB interface or even a RAM window in uVision I see this jump of 4 bit back in address. Thanks for the mode set up. What's still confusing me is 'LPC_EMC-&amp;gt;DYNAMICREFRESH'. When I read the manual I should use '7.8us * 204MHz/2 / 16(+1) cycl'. But in examples I see two programmings where the second call deals with '15625'. I have no clue where this number is coming from. Additionally, I do not see how examples matches the initialization procedure in the RAM data sheet. It talks about two 'AUTO REFRESH' cycles. I assume this is the 'PALL' command. I see only one. But I see multiple NOP commands. What are they doing? This is the magic I mean ;-))&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Greetings,&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:02:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/4-x-SDRAM-at-LPC43x7/m-p/578989#M19926</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:02:12Z</dc:date>
    </item>
  </channel>
</rss>