<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: LPC 811 image build using LPCExpresso Image size 178KB</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-811-image-build-using-LPCExpresso-Image-size-178KB/m-p/578958#M19922</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;got it Thank you&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it worked. Actually its generating axf file which is huge , and now I generated .bin and its below 7KB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the suppor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Jun 2016 10:22:37 GMT</pubDate>
    <dc:creator>ravikumarkadiya</dc:creator>
    <dc:date>2016-06-28T10:22:37Z</dc:date>
    <item>
      <title>LPC 811 image build using LPCExpresso Image size 178KB</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-811-image-build-using-LPCExpresso-Image-size-178KB/m-p/578954#M19918</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;we are usign LPC811 in one of our product, we lost our existing build setup and trying to build the LPC project. dowloaded LPCExpresso and tried to build the project iam able to build but the image size is huge at 178KB, our actual images are supposed to be 6 to 7KB not sure why this is happening&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Jun 2016 18:11:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-811-image-build-using-LPCExpresso-Image-size-178KB/m-p/578954#M19918</guid>
      <dc:creator>ravikumarkadiya</dc:creator>
      <dc:date>2016-06-27T18:11:12Z</dc:date>
    </item>
    <item>
      <title>Re: LPC 811 image build using LPCExpresso Image size 178KB</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-811-image-build-using-LPCExpresso-Image-size-178KB/m-p/578955#M19919</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That's unfortunate. I'd recommend you build an LPC811 wizard project to get a starting point for your build settings. It's possible you're building with no optimization, or the linker is not eliminating dead (unused) code from your image. This is the --gc-sections option in C/C++ Build -&amp;gt; Settings -&amp;gt; MCU Linker -&amp;gt; Miscellaneous. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;LPCXpresso Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Jun 2016 18:27:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-811-image-build-using-LPCExpresso-Image-size-178KB/m-p/578955#M19919</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2016-06-27T18:27:46Z</dc:date>
    </item>
    <item>
      <title>Re: LPC 811 image build using LPCExpresso Image size 178KB</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-811-image-build-using-LPCExpresso-Image-size-178KB/m-p/578956#M19920</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;we tried optimization as well with optimization it comes down to 75KB&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards,&lt;/P&gt;&lt;P&gt;Ravi&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Jun 2016 18:31:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-811-image-build-using-LPCExpresso-Image-size-178KB/m-p/578956#M19920</guid>
      <dc:creator>ravikumarkadiya</dc:creator>
      <dc:date>2016-06-27T18:31:00Z</dc:date>
    </item>
    <item>
      <title>Re: LPC 811 image build using LPCExpresso Image size 178KB</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-811-image-build-using-LPCExpresso-Image-size-178KB/m-p/578957#M19921</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How are you measuring the size? If you are looking at the file size, that has nothing to do do with the flash size. Suggest you read this faq&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/388954"&gt;Application Flash / RAM size&lt;/A&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 27 Jun 2016 19:16:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-811-image-build-using-LPCExpresso-Image-size-178KB/m-p/578957#M19921</guid>
      <dc:creator>thefallguy</dc:creator>
      <dc:date>2016-06-27T19:16:06Z</dc:date>
    </item>
    <item>
      <title>Re: LPC 811 image build using LPCExpresso Image size 178KB</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-811-image-build-using-LPCExpresso-Image-size-178KB/m-p/578958#M19922</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;got it Thank you&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it worked. Actually its generating axf file which is huge , and now I generated .bin and its below 7KB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the suppor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jun 2016 10:22:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-811-image-build-using-LPCExpresso-Image-size-178KB/m-p/578958#M19922</guid>
      <dc:creator>ravikumarkadiya</dc:creator>
      <dc:date>2016-06-28T10:22:37Z</dc:date>
    </item>
  </channel>
</rss>