<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC4337 USB1 project</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-USB1-project/m-p/578953#M19917</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by andres.cass on Sat Oct 31 05:55:48 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am starting with the USB stack in the LPC4337, but I have a problem. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am trying to make a simple virtual COM device with an eco functionality. I take the example base of the LPCOpen usbd_rom_cdc_uart but using the uC USB1 port.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;But when I run the application it gets stuck in &lt;/SPAN&gt;&lt;I&gt;while (!(Chip_Clock_GetPLLStatus(CGU_USB_PLL) &amp;amp; CGU_PLL_LOCKED)) {}&lt;/I&gt;&lt;SPAN&gt;while cicle inside the &lt;/SPAN&gt;&lt;I&gt;static void Chip_USB_PllSetup(void)&lt;/I&gt;&lt;SPAN&gt; function. It's like it can´t set the PLL for the USB.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Here is my code:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;main function&lt;/STRONG&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;int main(void) {

#if defined (__USE_LPCOPEN)
#if !defined(NO_BOARD_LIB)
&amp;nbsp;&amp;nbsp;&amp;nbsp; // Read clock settings and update SystemCoreClock variable
&amp;nbsp;&amp;nbsp;&amp;nbsp; SystemCoreClockUpdate();
&amp;nbsp;&amp;nbsp;&amp;nbsp; // Set up and initialize all required blocks and
&amp;nbsp;&amp;nbsp;&amp;nbsp; // functions related to the board hardware
&amp;nbsp;&amp;nbsp;&amp;nbsp; Board_Init();
&amp;nbsp;&amp;nbsp;&amp;nbsp; // Set the LED to the state of "On"
&amp;nbsp;&amp;nbsp;&amp;nbsp; Board_LED_Set(0, true);
#endif
#endif
&amp;nbsp;&amp;nbsp;&amp;nbsp; uint32_t sarasa = 0;
&amp;nbsp;&amp;nbsp;&amp;nbsp; while(sarasa &amp;lt; 10000)
&amp;nbsp;&amp;nbsp;&amp;nbsp; sarasa++;

&amp;nbsp;&amp;nbsp;&amp;nbsp; SystemCoreClockUpdate();

&amp;nbsp;&amp;nbsp;&amp;nbsp; USBD_API_INIT_PARAM_T usb_param;
USB_CORE_DESCS_T desc;
ErrorCode_t ret = LPC_OK;
USB_CORE_CTRL_T *pCtrl;

Chip_SCU_PinMuxSet(0x9, 5, (SCU_MODE_PULLUP | SCU_MODE_INBUFF_EN | SCU_MODE_FUNC2));/* P9_5 USB1_VBUS_EN, USB1 VBus function */
Chip_SCU_PinMuxSet(0x2, 5, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_FUNC2));/* P2_5 USB1_VBUS, MUST CONFIGURE THIS SIGNAL FOR USB1 NORMAL OPERATION */
Chip_SCU_PinMuxSet(0x6, 3, (SCU_MODE_PULLUP | SCU_MODE_INBUFF_EN | SCU_MODE_FUNC1));/* P6_3 USB0_PWR_EN, USB0 VBus function */

Chip_USB1_Init(); //USB_init_pin_clk();

/* Init USB API structure */
g_pUsbApi = (const USBD_API_T *) LPC_ROM_API-&amp;gt;usbdApiBase;

/* initialize call back structures */
memset((void *) &amp;amp;usb_param, 0, sizeof(USBD_API_INIT_PARAM_T));
usb_param.usb_reg_base = LPC_USB_BASE;
usb_param.max_num_ep = 4;
usb_param.mem_base = USB_STACK_MEM_BASE;
usb_param.mem_size = USB_STACK_MEM_SIZE;

/* Set the USB descriptors */
desc.device_desc = (uint8_t *) USB_DeviceDescriptor;
desc.string_desc = (uint8_t *) USB_StringDescriptor;

#ifdef USE_USB0
desc.high_speed_desc = USB_HsConfigDescriptor;
desc.full_speed_desc = USB_FsConfigDescriptor;
desc.device_qualifier = (uint8_t *) USB_DeviceQualifier;
#else
/* Note, to pass USBCV test full-speed only devices should have both
 * descriptor arrays point to same location and device_qualifier set
 * to 0.
 */
desc.high_speed_desc = USB_FsConfigDescriptor;
desc.full_speed_desc = USB_FsConfigDescriptor;
desc.device_qualifier = 0;
#endif

ret = USBD_API-&amp;gt;hw-&amp;gt;Init(&amp;amp;g_hUsb, &amp;amp;desc, &amp;amp;usb_param);
if (ret == LPC_OK) {

/*WORKAROUND for artf45032 ROM driver BUG:
Due to a race condition there is the chance that a second NAK event will
occur before the default endpoint0 handler has completed its preparation
of the DMA engine for the first NAK event. This can cause certain fields
in the DMA descriptors to be in an invalid state when the USB controller
reads them, thereby causing a hang.
 */
pCtrl = (USB_CORE_CTRL_T *) g_hUsb;/* convert the handle to control structure */
g_Ep0BaseHdlr = pCtrl-&amp;gt;ep_event_hdlr[0];/* retrieve the default EP0_OUT handler */
pCtrl-&amp;gt;ep_event_hdlr[0] = EP0_patch;/* set our patch routine as EP0_OUT handler */

/* Init UCOM - USB to UART bridge interface */
ret = UCOM_init(g_hUsb, &amp;amp;desc, &amp;amp;usb_param);
if (ret == LPC_OK) {
/* Make sure USB and UART IRQ priorities are same for this example */
NVIC_SetPriority(LPC_USB_IRQ, 1);
/*&amp;nbsp; enable USB interrupts */
NVIC_EnableIRQ(LPC_USB_IRQ);
/* now connect */
USBD_API-&amp;gt;hw-&amp;gt;Connect(g_hUsb, 1);
}
}


&amp;nbsp;&amp;nbsp;&amp;nbsp; // TODO: insert code here
&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Setup GPIOs for USB demos */
&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_SCU_PinMuxSet(0x9, 5, (SCU_MODE_PULLUP | SCU_MODE_INBUFF_EN | SCU_MODE_FUNC2));/* P9_5 USB1_VBUS_EN, USB1 VBus function */
&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_SCU_PinMuxSet(0x2, 5, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_FUNC2));/* P2_5 USB1_VBUS, MUST CONFIGURE THIS SIGNAL FOR USB1 NORMAL OPERATION */
&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_SCU_PinMuxSet(0x6, 3, (SCU_MODE_PULLUP | SCU_MODE_INBUFF_EN | SCU_MODE_FUNC1));/* P6_3 USB0_PWR_EN, USB0 VBus function */

&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_SCU_PinMuxSet(0xE, 7, (SCU_MODE_FUNC4 | SCU_MODE_PULLDOWN));
&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_GPIO_SetPinDIROutput(LPC_GPIO_PORT, 7, 7);

&amp;nbsp;&amp;nbsp;&amp;nbsp; // Force the counter to be placed into memory
&amp;nbsp;&amp;nbsp;&amp;nbsp; volatile static uint32_t i = 0 ;
&amp;nbsp;&amp;nbsp;&amp;nbsp; // Enter an infinite loop, just incrementing a counter
&amp;nbsp;&amp;nbsp;&amp;nbsp; while(1) {
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; i++ ;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if(i == 500000)
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; {
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_GPIO_SetPinToggle(LPC_GPIO_PORT, 7, 7);
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; i = 0;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }
&amp;nbsp;&amp;nbsp;&amp;nbsp; }
&amp;nbsp;&amp;nbsp;&amp;nbsp; return 0 ;
}&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;Chip_USB1_Init function&lt;/STRONG&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;void Chip_USB1_Init(void)
{
/* Setup and enable the PLL */
Chip_USB_PllSetup();

/* USB1 needs a 60MHz clock. To get it, a divider of 4 and then 2 are
&amp;nbsp;&amp;nbsp; chained to make a divide by 8 function. Connect the output of
&amp;nbsp;&amp;nbsp; divider D to the USB1 base clock. */
Chip_Clock_SetDivider(CLK_IDIV_A, CLKIN_USBPLL, 4);
Chip_Clock_SetDivider(CLK_IDIV_D, CLKIN_IDIVA, 2);
Chip_Clock_SetBaseClock(CLK_BASE_USB1, CLKIN_IDIVD, true, true);

/* enable USB main clock */
Chip_Clock_EnableBaseClock(CLK_BASE_USB1);
Chip_Clock_EnableOpts(CLK_MX_USB1, true, true, 1);
/* enable USB1_DP and USB1_DN on chip FS phy.*/
LPC_SCU-&amp;gt;SFSUSB = 0x12;
}&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;It never get out of that function so the application never works. How the PLL has to be setted?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you in advance.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:02:58 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:02:58Z</dc:date>
    <item>
      <title>LPC4337 USB1 project</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-USB1-project/m-p/578953#M19917</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by andres.cass on Sat Oct 31 05:55:48 MST 2015&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am starting with the USB stack in the LPC4337, but I have a problem. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I am trying to make a simple virtual COM device with an eco functionality. I take the example base of the LPCOpen usbd_rom_cdc_uart but using the uC USB1 port.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;But when I run the application it gets stuck in &lt;/SPAN&gt;&lt;I&gt;while (!(Chip_Clock_GetPLLStatus(CGU_USB_PLL) &amp;amp; CGU_PLL_LOCKED)) {}&lt;/I&gt;&lt;SPAN&gt;while cicle inside the &lt;/SPAN&gt;&lt;I&gt;static void Chip_USB_PllSetup(void)&lt;/I&gt;&lt;SPAN&gt; function. It's like it can´t set the PLL for the USB.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Here is my code:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;main function&lt;/STRONG&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;int main(void) {

#if defined (__USE_LPCOPEN)
#if !defined(NO_BOARD_LIB)
&amp;nbsp;&amp;nbsp;&amp;nbsp; // Read clock settings and update SystemCoreClock variable
&amp;nbsp;&amp;nbsp;&amp;nbsp; SystemCoreClockUpdate();
&amp;nbsp;&amp;nbsp;&amp;nbsp; // Set up and initialize all required blocks and
&amp;nbsp;&amp;nbsp;&amp;nbsp; // functions related to the board hardware
&amp;nbsp;&amp;nbsp;&amp;nbsp; Board_Init();
&amp;nbsp;&amp;nbsp;&amp;nbsp; // Set the LED to the state of "On"
&amp;nbsp;&amp;nbsp;&amp;nbsp; Board_LED_Set(0, true);
#endif
#endif
&amp;nbsp;&amp;nbsp;&amp;nbsp; uint32_t sarasa = 0;
&amp;nbsp;&amp;nbsp;&amp;nbsp; while(sarasa &amp;lt; 10000)
&amp;nbsp;&amp;nbsp;&amp;nbsp; sarasa++;

&amp;nbsp;&amp;nbsp;&amp;nbsp; SystemCoreClockUpdate();

&amp;nbsp;&amp;nbsp;&amp;nbsp; USBD_API_INIT_PARAM_T usb_param;
USB_CORE_DESCS_T desc;
ErrorCode_t ret = LPC_OK;
USB_CORE_CTRL_T *pCtrl;

Chip_SCU_PinMuxSet(0x9, 5, (SCU_MODE_PULLUP | SCU_MODE_INBUFF_EN | SCU_MODE_FUNC2));/* P9_5 USB1_VBUS_EN, USB1 VBus function */
Chip_SCU_PinMuxSet(0x2, 5, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_FUNC2));/* P2_5 USB1_VBUS, MUST CONFIGURE THIS SIGNAL FOR USB1 NORMAL OPERATION */
Chip_SCU_PinMuxSet(0x6, 3, (SCU_MODE_PULLUP | SCU_MODE_INBUFF_EN | SCU_MODE_FUNC1));/* P6_3 USB0_PWR_EN, USB0 VBus function */

Chip_USB1_Init(); //USB_init_pin_clk();

/* Init USB API structure */
g_pUsbApi = (const USBD_API_T *) LPC_ROM_API-&amp;gt;usbdApiBase;

/* initialize call back structures */
memset((void *) &amp;amp;usb_param, 0, sizeof(USBD_API_INIT_PARAM_T));
usb_param.usb_reg_base = LPC_USB_BASE;
usb_param.max_num_ep = 4;
usb_param.mem_base = USB_STACK_MEM_BASE;
usb_param.mem_size = USB_STACK_MEM_SIZE;

/* Set the USB descriptors */
desc.device_desc = (uint8_t *) USB_DeviceDescriptor;
desc.string_desc = (uint8_t *) USB_StringDescriptor;

#ifdef USE_USB0
desc.high_speed_desc = USB_HsConfigDescriptor;
desc.full_speed_desc = USB_FsConfigDescriptor;
desc.device_qualifier = (uint8_t *) USB_DeviceQualifier;
#else
/* Note, to pass USBCV test full-speed only devices should have both
 * descriptor arrays point to same location and device_qualifier set
 * to 0.
 */
desc.high_speed_desc = USB_FsConfigDescriptor;
desc.full_speed_desc = USB_FsConfigDescriptor;
desc.device_qualifier = 0;
#endif

ret = USBD_API-&amp;gt;hw-&amp;gt;Init(&amp;amp;g_hUsb, &amp;amp;desc, &amp;amp;usb_param);
if (ret == LPC_OK) {

/*WORKAROUND for artf45032 ROM driver BUG:
Due to a race condition there is the chance that a second NAK event will
occur before the default endpoint0 handler has completed its preparation
of the DMA engine for the first NAK event. This can cause certain fields
in the DMA descriptors to be in an invalid state when the USB controller
reads them, thereby causing a hang.
 */
pCtrl = (USB_CORE_CTRL_T *) g_hUsb;/* convert the handle to control structure */
g_Ep0BaseHdlr = pCtrl-&amp;gt;ep_event_hdlr[0];/* retrieve the default EP0_OUT handler */
pCtrl-&amp;gt;ep_event_hdlr[0] = EP0_patch;/* set our patch routine as EP0_OUT handler */

/* Init UCOM - USB to UART bridge interface */
ret = UCOM_init(g_hUsb, &amp;amp;desc, &amp;amp;usb_param);
if (ret == LPC_OK) {
/* Make sure USB and UART IRQ priorities are same for this example */
NVIC_SetPriority(LPC_USB_IRQ, 1);
/*&amp;nbsp; enable USB interrupts */
NVIC_EnableIRQ(LPC_USB_IRQ);
/* now connect */
USBD_API-&amp;gt;hw-&amp;gt;Connect(g_hUsb, 1);
}
}


&amp;nbsp;&amp;nbsp;&amp;nbsp; // TODO: insert code here
&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Setup GPIOs for USB demos */
&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_SCU_PinMuxSet(0x9, 5, (SCU_MODE_PULLUP | SCU_MODE_INBUFF_EN | SCU_MODE_FUNC2));/* P9_5 USB1_VBUS_EN, USB1 VBus function */
&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_SCU_PinMuxSet(0x2, 5, (SCU_MODE_INACT | SCU_MODE_INBUFF_EN | SCU_MODE_ZIF_DIS | SCU_MODE_FUNC2));/* P2_5 USB1_VBUS, MUST CONFIGURE THIS SIGNAL FOR USB1 NORMAL OPERATION */
&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_SCU_PinMuxSet(0x6, 3, (SCU_MODE_PULLUP | SCU_MODE_INBUFF_EN | SCU_MODE_FUNC1));/* P6_3 USB0_PWR_EN, USB0 VBus function */

&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_SCU_PinMuxSet(0xE, 7, (SCU_MODE_FUNC4 | SCU_MODE_PULLDOWN));
&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_GPIO_SetPinDIROutput(LPC_GPIO_PORT, 7, 7);

&amp;nbsp;&amp;nbsp;&amp;nbsp; // Force the counter to be placed into memory
&amp;nbsp;&amp;nbsp;&amp;nbsp; volatile static uint32_t i = 0 ;
&amp;nbsp;&amp;nbsp;&amp;nbsp; // Enter an infinite loop, just incrementing a counter
&amp;nbsp;&amp;nbsp;&amp;nbsp; while(1) {
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; i++ ;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if(i == 500000)
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; {
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Chip_GPIO_SetPinToggle(LPC_GPIO_PORT, 7, 7);
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; i = 0;
&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }
&amp;nbsp;&amp;nbsp;&amp;nbsp; }
&amp;nbsp;&amp;nbsp;&amp;nbsp; return 0 ;
}&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;STRONG&gt;Chip_USB1_Init function&lt;/STRONG&gt;&lt;BR /&gt;&lt;TABLE border="1"&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD bgcolor="#cacaca"&gt; &lt;PRE&gt;void Chip_USB1_Init(void)
{
/* Setup and enable the PLL */
Chip_USB_PllSetup();

/* USB1 needs a 60MHz clock. To get it, a divider of 4 and then 2 are
&amp;nbsp;&amp;nbsp; chained to make a divide by 8 function. Connect the output of
&amp;nbsp;&amp;nbsp; divider D to the USB1 base clock. */
Chip_Clock_SetDivider(CLK_IDIV_A, CLKIN_USBPLL, 4);
Chip_Clock_SetDivider(CLK_IDIV_D, CLKIN_IDIVA, 2);
Chip_Clock_SetBaseClock(CLK_BASE_USB1, CLKIN_IDIVD, true, true);

/* enable USB main clock */
Chip_Clock_EnableBaseClock(CLK_BASE_USB1);
Chip_Clock_EnableOpts(CLK_MX_USB1, true, true, 1);
/* enable USB1_DP and USB1_DN on chip FS phy.*/
LPC_SCU-&amp;gt;SFSUSB = 0x12;
}&lt;/PRE&gt; &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;It never get out of that function so the application never works. How the PLL has to be setted?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Thank you in advance.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:02:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4337-USB1-project/m-p/578953#M19917</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:02:58Z</dc:date>
    </item>
  </channel>
</rss>