<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC4357 TFT Display 4Bit each colour without external RAM</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357-TFT-Display-4Bit-each-colour-without-external-RAM/m-p/578843#M19898</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Martin84 on Tue Dec 02 02:53:08 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Which TFT is it? May be a Sainsmart-TFT? I think your TFT has an internal LCD Controller (i.e. SSD1289) which you drive with the 16-bit HW-Interface. These LCD Controllers have a internal RAM as Framebuffer which you can use. But I don't know if you can use this TFT-Framebuffer with the LPC LCD-Controller. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If there's such a LCD-Controller like the SSD1289 you can drive the TFT with the LPC EMC or with GPIO-Lines.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Martin&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:05:00 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:05:00Z</dc:date>
    <item>
      <title>LPC4357 TFT Display 4Bit each colour without external RAM</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357-TFT-Display-4Bit-each-colour-without-external-RAM/m-p/578842#M19897</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Georg on Mon Dec 01 01:04:57 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;i use a LPC4357 with a small TFT (320x240) display. This display is connected over 16Bit HW-Interface &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;and work fine. But for this funktion i need a external ram for the framebuffer.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I need a solution to run this TFT without external RAM. I would use it with 4bit each colour.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;But i don't understand how to initialise the colourpalette for this mode.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can someone give me some examples or help to initialise the tft.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Cursor works fine in 4Bit mode.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thx.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Georg.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:04:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357-TFT-Display-4Bit-each-colour-without-external-RAM/m-p/578842#M19897</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:04:59Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4357 TFT Display 4Bit each colour without external RAM</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357-TFT-Display-4Bit-each-colour-without-external-RAM/m-p/578843#M19898</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Martin84 on Tue Dec 02 02:53:08 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Which TFT is it? May be a Sainsmart-TFT? I think your TFT has an internal LCD Controller (i.e. SSD1289) which you drive with the 16-bit HW-Interface. These LCD Controllers have a internal RAM as Framebuffer which you can use. But I don't know if you can use this TFT-Framebuffer with the LPC LCD-Controller. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;If there's such a LCD-Controller like the SSD1289 you can drive the TFT with the LPC EMC or with GPIO-Lines.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Martin&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:05:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357-TFT-Display-4Bit-each-colour-without-external-RAM/m-p/578843#M19898</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:05:00Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4357 TFT Display 4Bit each colour without external RAM</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357-TFT-Display-4Bit-each-colour-without-external-RAM/m-p/578844#M19899</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Georg on Tue Dec 02 03:47:15 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;i Use a Onation OT035AQDDDT display with a HX8238 controller onbaord.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I drive this display wit the 16-bit HW-Interface and i use the lcd-controller from lpc.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;For framebuffer i use the external RAM. But i need a solution without ext. RAM.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;4Bit colourdepth is enough for my application.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I can configure the lpc lcd-controller to work with 4Bit. But i can not display some&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;colours. Only the cursor for my touch works and is displayed on lcd.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thx.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regard,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Georg.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:05:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357-TFT-Display-4Bit-each-colour-without-external-RAM/m-p/578844#M19899</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:05:01Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4357 TFT Display 4Bit each colour without external RAM</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357-TFT-Display-4Bit-each-colour-without-external-RAM/m-p/578845#M19900</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Georg on Mon Dec 15 03:56:18 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;i need only to know how to config the LCD-Controller from LPC and the&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Color Palette registers to run my display with 4 Bit and so save memory.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Ich will only use internal memory of LPC µC.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thx.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Georg.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:05:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357-TFT-Display-4Bit-each-colour-without-external-RAM/m-p/578845#M19900</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:05:01Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4357 TFT Display 4Bit each colour without external RAM</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357-TFT-Display-4Bit-each-colour-without-external-RAM/m-p/1193520#M43146</link>
      <description>&lt;P&gt;How did you manage to do so?&lt;/P&gt;</description>
      <pubDate>Thu, 03 Dec 2020 23:23:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4357-TFT-Display-4Bit-each-colour-without-external-RAM/m-p/1193520#M43146</guid>
      <dc:creator>magdiel3</dc:creator>
      <dc:date>2020-12-03T23:23:32Z</dc:date>
    </item>
  </channel>
</rss>