<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックADC configuration for  ADC1_7 pin</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-configuration-for-ADC1-7-pin/m-p/576518#M19448</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by LPC_beginner on Sun Jun 23 04:30:32 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;I am very new to&amp;nbsp;LPC43xx series processors. My problem is with reading ADC&amp;nbsp; using a specific channel.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;After going thorough the user guide and examples provided, I have come up with following steps.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;nbsp;/* get scu base&amp;nbsp; */&lt;BR /&gt;&amp;nbsp;p = (LPC_SCU_Type*)(LPC_SCU_BASE);&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;nbsp;/*&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;nbsp; *&amp;nbsp; Select ADC function&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;nbsp; */&lt;BR /&gt;&amp;nbsp;p-&amp;amp;gt;ENAIO1 |= 0x80; //Enable ADC function for&amp;nbsp; ADC1_7 (pad PF_7 in BGA256 package)&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;/* &lt;BR /&gt;&amp;nbsp; * Disable internal pullup&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;* Disable internal pull down&amp;nbsp;&lt;BR /&gt;&amp;nbsp; * Select&amp;nbsp;&amp;nbsp;function &amp;nbsp;as&amp;nbsp;GPIO&lt;BR /&gt;&amp;nbsp; */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;p-&amp;amp;gt;SFSPF_7 = 0x14; //&amp;nbsp;Is this configuration is correct??&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;/* Set GPIO as input mode */&lt;BR /&gt;&amp;nbsp;GPIO_SetDir(GPIO_PORT_7,(1&amp;amp;lt;&amp;amp;lt; 21), INPUT_MODE);&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;/*&amp;nbsp;disable band gap option&amp;nbsp;*/ &lt;BR /&gt;&amp;nbsp; p-&amp;amp;gt;ENAIO2 = 0;&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;nbsp;/* ADC initialize */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;ADC_Init(LPC_ADC1, 200000, 10); /* Initialize ADC1 */&lt;BR /&gt;&amp;nbsp;/* Disable ADC Interrupt *&amp;nbsp;&lt;BR /&gt;&amp;nbsp;ADC_IntConfig(LPC_ADC1,ADC_ADINTEN7,DISABLE);&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;nbsp;ADC_ChannelCmd(LPC_ADC1,ADC_CHANNEL_7,ENABLE);&lt;BR /&gt;&amp;nbsp;ADC_StartCmd(LPC_ADC1,ADC_START_NOW);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;/*&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; * Wait for conversion&amp;nbsp;to complete&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;while (!(ADC_ChannelGetStatus(LPC_ADC1,ADC_CHANNEL_7,ADC_DATA_DONE)));&lt;BR /&gt;&amp;nbsp;&amp;nbsp;ADC_val = ADC_ChannelGetData(LPC_ADC0,ADC_CHANNEL_7);&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;}&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;I have measured the pad PF_2&amp;nbsp; which is having voltage of 1.56, but&amp;nbsp; I always get 0 in adc register.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Verified that&amp;nbsp;&amp;nbsp;DONE bit is getting set after the adc conversion start.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Do I missed any initialization.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Appreciate any pointers on this issue...&lt;/P&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 19:01:55 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T19:01:55Z</dc:date>
    <item>
      <title>ADC configuration for  ADC1_7 pin</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-configuration-for-ADC1-7-pin/m-p/576518#M19448</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by LPC_beginner on Sun Jun 23 04:30:32 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;P&gt;I am very new to&amp;nbsp;LPC43xx series processors. My problem is with reading ADC&amp;nbsp; using a specific channel.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;After going thorough the user guide and examples provided, I have come up with following steps.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;nbsp;/* get scu base&amp;nbsp; */&lt;BR /&gt;&amp;nbsp;p = (LPC_SCU_Type*)(LPC_SCU_BASE);&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;nbsp;/*&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;nbsp; *&amp;nbsp; Select ADC function&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;nbsp; */&lt;BR /&gt;&amp;nbsp;p-&amp;amp;gt;ENAIO1 |= 0x80; //Enable ADC function for&amp;nbsp; ADC1_7 (pad PF_7 in BGA256 package)&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;/* &lt;BR /&gt;&amp;nbsp; * Disable internal pullup&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;* Disable internal pull down&amp;nbsp;&lt;BR /&gt;&amp;nbsp; * Select&amp;nbsp;&amp;nbsp;function &amp;nbsp;as&amp;nbsp;GPIO&lt;BR /&gt;&amp;nbsp; */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;p-&amp;amp;gt;SFSPF_7 = 0x14; //&amp;nbsp;Is this configuration is correct??&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;/* Set GPIO as input mode */&lt;BR /&gt;&amp;nbsp;GPIO_SetDir(GPIO_PORT_7,(1&amp;amp;lt;&amp;amp;lt; 21), INPUT_MODE);&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;/*&amp;nbsp;disable band gap option&amp;nbsp;*/ &lt;BR /&gt;&amp;nbsp; p-&amp;amp;gt;ENAIO2 = 0;&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;nbsp;/* ADC initialize */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;ADC_Init(LPC_ADC1, 200000, 10); /* Initialize ADC1 */&lt;BR /&gt;&amp;nbsp;/* Disable ADC Interrupt *&amp;nbsp;&lt;BR /&gt;&amp;nbsp;ADC_IntConfig(LPC_ADC1,ADC_ADINTEN7,DISABLE);&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;nbsp;ADC_ChannelCmd(LPC_ADC1,ADC_CHANNEL_7,ENABLE);&lt;BR /&gt;&amp;nbsp;ADC_StartCmd(LPC_ADC1,ADC_START_NOW);&lt;BR /&gt;&amp;nbsp;&amp;nbsp;/*&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; * Wait for conversion&amp;nbsp;to complete&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;while (!(ADC_ChannelGetStatus(LPC_ADC1,ADC_CHANNEL_7,ADC_DATA_DONE)));&lt;BR /&gt;&amp;nbsp;&amp;nbsp;ADC_val = ADC_ChannelGetData(LPC_ADC0,ADC_CHANNEL_7);&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;}&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;I have measured the pad PF_2&amp;nbsp; which is having voltage of 1.56, but&amp;nbsp; I always get 0 in adc register.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Verified that&amp;nbsp;&amp;nbsp;DONE bit is getting set after the adc conversion start.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Do I missed any initialization.&lt;/P&gt;&lt;BR /&gt;&lt;P&gt;Appreciate any pointers on this issue...&lt;/P&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 19:01:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/ADC-configuration-for-ADC1-7-pin/m-p/576518#M19448</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T19:01:55Z</dc:date>
    </item>
  </channel>
</rss>